Post Go back to editing

Output waveform is distorted

Thread Summary

The user is experiencing distorted sine wave output from a custom board with AD9747 DAC interfaced with a Zynq MPSoC FPGA, especially at higher frequencies. The final answer suggests checking the clock input for noise, verifying the timing of data transfer from the FPGA to the DAC, and using the AD9747 Evaluation Board as a reference. The user confirmed the resistor values are 50 ohms, and the output is heavily distorted in the frequency domain. Additional troubleshooting steps include verifying the LMK04828 configuration for low jitter and proper PLL loop bandwidth, and ensuring correct balun connections.
AI Generated Content
Category: Hardware
Product Number: AD9747

Greetings. 

I have a custom board which has AD9747 DAC interfaced with FPGA. I'm sampling the DAC with 100 MHz clock & generating sine wave from FPGA. However the waveform looks distorted & not smooth. 

This is 10 MHz sine wave output (DCO is 100 MHz)

However, as I keep increasing frequency, the output is getting heavily distorted. 

Currently, I'm not using any filters at the output. 

Thanks & Regards, 

Srujan Vedula 

  • Hi  ,

    Thank you for your interest in AD9747.  will look into this query and get back to you as soon as possible.

    Are you using the AD9747 Evaluation Board? If not, can you please provide your schematic? Also, where are you getting the DACCLK from and what FPGA board are you using? 

    Best regards,
    Marco

  • Hi Marco,

    Thanks for the reply. 

    I’m working on a fully custom board where the DACCLK for the AD9747 is being generated by an LMK04828 clock generator. The FPGA used in the design is a Zynq MPSoC.

    Here is the schematic of AD9747. 

    Thanks & Regards,

    Srujan 

  • Hi  ,

    Do you have a frequency domain capture? It would be best to see which frequencies are showing at the output causing the waveform to be distorted. Kindly check if there are ripple noise from the supply rails and noise coming from the clock pins. 

    Best regards,
    Marco

  • Hi  ,

    Additionally, could you please confirm the values of R30, R31, R36, and R37 (RLOADs)? Based on the schematic diagram you provided, they appear to be 50 kΩ. However, the EVB schematic shows 49.9 Ω resistors installed, which you may follow for consistency.


    Regarding the distorted output that worsens with increasing DCO frequency, please try reconfiguring the DAC after changing the DCO frequency, or perform a power cycle on your setup to see if that resolves the issue.

    Thanks and kind regards,

    Alex

  • Hi Alex,

    The Resistor values are 50 ohm. Not 50k ohm. 

    It looks heavily distorted when I view in spectrum analyser. 

  • Hi Marco,

    Here I'm attaching the video. 

    Signal Frequency = 50MHz

    Sampling Frequency = 200 MHz 

    Thanks & Regards,

    Srujan Vedula 

  • Hi  ,

    Apologies for the delayed response.  If this issue is not yet resolved, you can check below items on your setup.

    • Output Stage
      • Just to ensure correct orientation or pin connections of the baluns, please help to follow the EVB schematic diagram.

      

    • Clock Integrity
      • Verify LMK04828 configuration: low jitter mode, proper PLL loop bandwidth.
      • Clock distribution as per Table 5 of rev C datasheet.

    Thanks and kind regards,

    Alex

  • Hi  ,

    The output does look to be heavily distorted, could you try lowering the output frequency and see if there's a range where there's no distortion? Try around <10MHz. 

    As suggested by Alex, you might want to check the clock input (LMK04828) and see if it's noisy. Are you using the default register values? If both are checked, the problem might be the timing of data transfer from your FPGA to the DAC (refer to Page 25 of Rev C datasheet). There isn't any issues with the schematic you sent, but you could the AD9747 Evaluation Board as reference for your design.

    Best regards,
    Marco

  • Hi Marco,

    Sorry for the late reply. 

    Right now I do not have the board to test but could you please clarify if any reconstruction filter required after DAC to smooth the waveform?

    Thanks & Regards,

    Srujan

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.