Post Go back to editing

AD9162-FMCC-EBZ and ZCU102 Rev 1.1 eval board mechanical compatibility

Thread Summary

The user is trying to interface an AD9162-FMCC-EBZ eval board with a ZCU102 Rev 1.1 eval board but is facing mechanical compatibility issues. The recommended solution is to use a VITA 57.4 FMC+ Extender Card from Samtec. The user will test this extender card to resolve the issue.
AI Generated Content
Category: Hardware
Product Number: AD9162-FMCC-EBZ, AD9162

Hello,

I am trying to interface an AD9162-FMCC-EBZ eval board with a ZCU102 Rev 1.1 eval board. Both boards contains FMC connectors with 400 pins and seem to be compatible with each other but I am unable to interface them mechanically.

My questions are:
1. Is the AD9162-FMCC-EBZ mechanically compatible with the ZCU102 eval board?
2. If not, could you recommend a specific FMC interposer or adapter to bridge this combination?
3. Are there any resources/notes regarding the pairing of these specific boards?

Thank you for your help,
Pranav

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.