Post Go back to editing

AD9162 boot loader pass bit low - reports engineering Revision

Category: Hardware
Product Number: AD9162

Hi all,

We follow the AD9162 DAC start-up sequence in Table 42, including setting up the SPI bus and configuring the NVRAM. Our board reports that the boot load pass bit (reg. 0x604 bit 1) is low. Upon looking into this I have noticed that the board reports unusual values for the product ID and revision.

Chip ID: 0x0000
DAC Chip Type: 4
DAC Product Grade: 0
DAC Product Revision: 6
I would have expected the product grade to be 0x004 = 0x62 and 0x005 = 0x91 if the NVRAM had been configured correctly (Table 42 note 1). Since the boot load pass bit is 0 indicating not successful I can understand why the product ID might still be 0x0000, but I would have expected the revision still to be 0x03. Is this a correct assumption? The AD916x source code indicates that any value other than 0x03 is an engineering release. Is this also correct?

We are using a custom dev board with our own driver software that is very similar to the AD916x driver. We can see it communicating just fine over SPI on the scope so I am confident that it not the SPI bus at fault. 

Our source code effectively looks like this:

write_reg(0x000, 0x18)

write_reg(0x0D2, 0x52)

write_reg(0x0D2, 0xD2)

write_reg(0x606, 0x02)

write_reg(0x607, 0x00)

write_reg(0x604, 0x01)

// sleep for 1000us

lock = read_reg(0x604) & 0x02

_chip_type = read_reg(0x003)

_chip_id = ((uint16_t) read_reg(0x004) << 0)  | ((uint16_t) read_reg(0x005) << 8)

uint8_t chip_grade_rev = read_reg(0x006)

_prod_grade = (chip_grade_rev >> 4)

_dev_revision = (chip_grade_rev & 0x0F)

Any guidance on what might be going wrong would be welcome.

Edit Notes

Clarifying reg values
[edited by: grawl at 10:28 AM (GMT -4) on 10 Sep 2025]

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.