Post Go back to editing

Problem of doing multichip synchronization

Thread Summary

The user is experiencing phase difference instability between two AD9142A DACs when changing the FTW value multiple times. The final answer suggests verifying the DLL lock status in Register 0x0E and using frame-initiated updates instead of SPI updates, as per the synchronization procedure for PLL Off. The user clarified that the DLL is disabled and the delay line is enabled due to the DCI rate of 160 MHz, and inquired about the necessity of enabling the DLL for synchronization and the relationship between the DLL and NCO FTW updates.
AI Generated Content
Category: Hardware
Product Number: AD9142A

Hi,

I am tring to synchronize multichip to generate two fixed phase difference signal. When two DACs are outputting signals in a stable sence, the phase difference stay stable; but when changing the value of  FTW for around 4 times, the phase difference between two signals change.

I am following the description of synchronization procedure for PLL off in the AD9142A datasheet. Here is my configuration of register: 

reg          input setting

0x28       0x02

0x31       FTW[7:0]

0x32       FTW[15:8]

0x33       FTW[23:16]

0x34       FTW[16:24]

0x30       0x11

0x25       0x01

0x42      0x41

0x27      0x50

0x22      0x0a

0x21      0x03

According to the description of the datasheet, the I can get a high value from 0x22[3], but the feedback information is different to the description. Here is the feedback information:

reg         reading back value

0x30        0x33

0x22        0x01

0x21        0x03

 

I wonder if my setting is right, or getting some suggestions of synchonizing multichip. I am grateful for suggestions and disscussion. Thank you!

 

Parents
  • Hi  ,

    Thank you for your interest in AD9142A. The DLL should be enabled and locked as per the synchronization procedure. Were you able to verify if the DLL is locked? This can be enabled in Register 0x0A and verify it's locked in Register 0x0E. 

    Also, since you will synchronize the NCO output from multiple devices, the frame-initiated update is recommended instead of the SPI initiated update as prescribed in Page 34 of the Rev B datasheet. In the Synchronization procedure for PLL Off described in Page 38, there's a bit of typo: Step 8 is supposed to be verify that Register 0x30[6] should read back 1 instead of Register 0x22[3] to verify that there's a complete Frame-initiated NCO FTW update. 

    Best regards,
    Marco

Reply
  • Hi  ,

    Thank you for your interest in AD9142A. The DLL should be enabled and locked as per the synchronization procedure. Were you able to verify if the DLL is locked? This can be enabled in Register 0x0A and verify it's locked in Register 0x0E. 

    Also, since you will synchronize the NCO output from multiple devices, the frame-initiated update is recommended instead of the SPI initiated update as prescribed in Page 34 of the Rev B datasheet. In the Synchronization procedure for PLL Off described in Page 38, there's a bit of typo: Step 8 is supposed to be verify that Register 0x30[6] should read back 1 instead of Register 0x22[3] to verify that there's a complete Frame-initiated NCO FTW update. 

    Best regards,
    Marco

Children
  • Hi Marco,

    Thank you for your reply. After I double checked the configration, I find that the the setting of the Register 0x0D to  0x16, and set the Register 0x0A to 0x0 to disable the DLL. 

    I set the DCI rate to 160MHz, which is not exceed 250MHz. So I follow the recommendation in Register 0x0D, disabled the DLL and enabled the delay line. Is it mandatory to enable the DLL for the synchronization, even if the DCI rate does not fast enough?

    Moreover, I want to know more about the relationship between the DLL and the synchronization. When looking at the functional block diagram, I notice that the DLL is working to the DCI directly, and the FTW is updated base on the DAC_CLK. Is theree any mutual influence between them?

    I am looking forward to your reply, thank you very much.

    Best regards,

    Allen

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.