Post Go back to editing

Problem of doing multichip synchronization

Thread Summary

The user is experiencing phase difference instability between two AD9142A DACs when changing the FTW value multiple times. The final answer suggests verifying the DLL lock status in Register 0x0E and using frame-initiated updates instead of SPI updates, as per the synchronization procedure for PLL Off. The user clarified that the DLL is disabled and the delay line is enabled due to the DCI rate of 160 MHz, and inquired about the necessity of enabling the DLL for synchronization and the relationship between the DLL and NCO FTW updates.
AI Generated Content
Category: Hardware
Product Number: AD9142A

Hi,

I am tring to synchronize multichip to generate two fixed phase difference signal. When two DACs are outputting signals in a stable sence, the phase difference stay stable; but when changing the value of  FTW for around 4 times, the phase difference between two signals change.

I am following the description of synchronization procedure for PLL off in the AD9142A datasheet. Here is my configuration of register: 

reg          input setting

0x28       0x02

0x31       FTW[7:0]

0x32       FTW[15:8]

0x33       FTW[23:16]

0x34       FTW[16:24]

0x30       0x11

0x25       0x01

0x42      0x41

0x27      0x50

0x22      0x0a

0x21      0x03

According to the description of the datasheet, the I can get a high value from 0x22[3], but the feedback information is different to the description. Here is the feedback information:

reg         reading back value

0x30        0x33

0x22        0x01

0x21        0x03

 

I wonder if my setting is right, or getting some suggestions of synchonizing multichip. I am grateful for suggestions and disscussion. Thank you!

 

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.