Post Go back to editing

AD9164: Disable unused lanes

Thread Summary

The user is sending constant zeros on some lanes of the AD9164 and wants to disable these lanes to save resources. Disabling lanes 1, 3, 5, and 7 in register 0x201 and routing active lanes in the cross-matrix worked in testing, but synchronization on K-symbols fails when the lanes are disabled in the FPGA. The issue may be related to the CDR failing on the inactive lanes, and the user is seeking a solution to maintain synchronization.
AI Generated Content
Category: Hardware
Product Number: AD9164

Hi!

On some lanes of the AD9164, I am constantly sending zeros. Is it possible to disable these lanes within the AD9164 to save resources in both the layout and the FPGA?

All LSB 7:0 are constant zero:

THX!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.