Post Go back to editing

Power of evaluation AD9175 -FMZ-EBZ and SPI communication

Thread Summary

The user inquired about configuring the DAC9175 eval board directly via the P3 header (SPI) without USB. The final answer confirmed that external power to TP41 and TP42 is sufficient, and suggested removing the jumper on JP71 to power down the PIC and USB port. The user also asked if connecting the ADS8 board and DAC1975 would still allow communication via P3, but this was not addressed in the final answer.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9175

Hi questions for DAC 9175 eval board:

1. if i want to configure only DAC9175 eval board directly via P3 header (SPI) do i need additional connection of USB to the board or enough to connect external power 12VDC via TP41 and GND TP2, and do i need additional changes in the evaluation board itself bypass PIC or something else.  


2. if i connect ADS8 board and DAC1975 can i still be able communicate via P3 connector, because schematic page 7. has note about connection USB and SPI bus control.

thanks,