AD9163
Recommended for New Designs
The AD91631 is a high performance, 16-bit digital-to-analog converter (DAC) that supports data rates to 6 GSPS. The DAC core is based on a quad-switch...
Datasheet
AD9163 on Analog.com
Hello,
I have a question about the settings for 0x151[2:0].
Register 0x151 has three bits.
Bit 2: SHUFFLE_MSB
Bit 1: SHUFFLE_ISB
Bit 0:SHUFFLE_DDR
I could not find a detailed description of these bits.
Could you please tell me what these bits are used for?
Best regards,
y_suzuki
Hi y_suzuki ,
The AD9175 has the same shuffle mode capability and includes a detailed explanation about MSB shuffling in its datasheet (pp. 66-67).

The AD9163 features 3 different shuffling techniques as seen in the table below. However, it is recommended that MSB shuffling be used whenever this mode is enabled.


Regards,
Zaeefa