Post Go back to editing

Max Frequency Characterized in Datasheet

Category: Datasheet/Specs
Product Number: AD9744

Hi,

The AD9744 is specified to clock to 210MHz, making the Nyquist frequency 105MHz. However the datasheet only characterises for a maximum output frequency of 69MHz. Is there a reason for characterising only up to 69MHz and not up to 105MHz?

I plan to use the DAC up to 90MHz and would like to know if there is a "hidden" limitation on maximum output frequency or will the device work till 90MHz (i.e work till it's theoretical limit of 105MHz) or not.

Thanks

Regards

Parents Reply Children
No Data