The datasheet for the AD9714/AD9715/AD9716/AD9717 states that these are pin compatible devices, but the pinouts for the IOUTP/IOUTN signals are different between the 14/15 and 16/17. It looks like maybe it is just a typo in the device symbol for the 14/15 in the datasheet. The symbol for the AD9714/15 actually does not agree with its own pin description table. I wanted to verify what the correct pinout is, but it seems the majority of the data agrees that pin 29 ought to be the N and 28 ought to be the P. If you can confirm that is correct, and possibly update the datasheet, that would be excellent. Thanks!