Post Go back to editing

Reading faulty chip temperature

Category: Hardware
Product Number: AD9162

Hi.

We are successfully using the AD9162. All is working fine.

However, sometimes we get faulty temperature readouts from the AD9162 after power up. Register 0x133 responds with 0x11 (normally it responds 0x94). 0x94 corresponds to a temperature around 48 °C, while 0x11 corresponds to around -164 °C.

Is there a minimum time required between writing to register 0x135 and 0x134?

Is there a minimum time between writing to register 0x134 and reading the result from 0x133+0x132?

Regards

Parents Reply Children
No Data