Post Go back to editing

Signal output selection with twos complement and offset binary digital

Category: Hardware
Product Number: MAX5878

xHello, the MAX5878 DAC has the TORI jumper JU3 pin for selection of two's complement output and offset binary digital output. Here i connected pin 1 and pin 2 for signed two's complement signal. I have attached the output of the oscilloscope, the hardware and the simulation picture. I want to get the signal as in the simulation. But i couldn't figure out. Previously i had generated the sine wave with this configuration.  I am confused at which point i am wrong is it on the FPGA side of the DAC side.? m