Post Go back to editing

PLL

Category: Datasheet/Specs
Product Number: AD9148

Hello, when I configured 9148, I ran into this problem:

frefclk = 120MHz,  fvco = 1920MHz, fdacclk = 480MHz

fdata = 240MHz, N0 = 4, N1 = 4, N2 = 16, pll enable, enable pll lock lost, enable pll lock, vco band manual mode is selected and reg ox0A is set to CC. However, the query value of 0x06 is 0x0f or 0x0b, which means that the pll lock fails but does not indicate lost.The output signal bandwidth is less than 200M.

plz help me,thanks.



edit PLL control 0 reg
[edited by: Lily0303 at 9:14 AM (GMT -4) on 6 Sep 2024]
Parents Reply Children
No Data