Post Go back to editing

AD9102 - DAC CONSTANT issue

Thread Summary

The user is unable to generate a DC current level at the output of AD9102 in DC CONSTANT mode despite configuring registers 0x27 and 0x31. The final answer suggests checking the Power Supply Notes in the datasheet and removing any components that might filter out the DC value, such as C507. The user confirms the issue persists even after removing C507 and setting the correct power supply voltages.
AI Generated Content
Category: Hardware
Product Number: AD9102

I am working with AD9102 but i am unable to see a DC current level at the output (DC CONSTANT mode). It seems that only Wave_CONFIG, address 0x27 and DAC_CST, address 0x31 needs to be configured but nothing goes out. 

SPI works good

Here is configuration:

SPICONFIG Reg 0x00 : 0x0000

WAV_CONFIG Reg0x27 : 0x0001

DAC_CST Reg 0x31 : 0xA300

See schematics attached 

Thanks

Parents Reply Children