The AD9163 chip has a working clock of 6GHz, a line rate of 7.5Gbit/s, and 204b parameters of F=1 and K=32.
When I am debugging the synchronization of 4 AD9163 chips, I access registers 0x037 and 0x038. The manual explains the phase relationship between the 4-fold DAC clock and the sampled SYSREF. So, how should I use this return value to achieve synchronization? Most of the return values are 0x0fe0, 0x0fc0, 0x0f80, 0x0f00. What do these values represent?