Post Go back to editing

How to use the QSIP write multibyte registers

Category: Datasheet/Specs
Product Number: AD3551R

Hi ADI Team,

I am using the AD3551R and have encountered some confusion regarding the multibyte register settings. In the section on 'Multibyte Registers', it is mentioned that multibyte registers can only be transferred in a single SPI transaction. However, when I need a fast rate and must update the DAC register data with QSPI, this seems contradictory. Am I missing some important details? I have tried to read the datasheet for answers but found nothing specific on this. I hope you can provide some clarification. Thank you very much.

  • Hi  ,

    This is to acknowledge your query. Please give the product owner ( ) a brief period to look into this and provide you with a response.

    Regards,
    Zaeefa

  • That specific note refers to the limitation of writing multi-byte registers partially. If a register has 2 or 3 bytes, all of them must be written within the same SPI transaction, otherwise an error is produced and the register remains unchanged.

    Note that multi-byte registers can only be written in descending order, therefore the starting address for register CH0_DAC_16B is 0x2A and data must be serialized starting from the MSB.

    The AD3551R allows writing multiple registers in a row. As long as CS is held low, the address pointer keeps decrementing with every data byte received. Therefore it is possible to write a block of contiguous registers in a single SPI frame, starting from the highest address.

    In addition to this, if streaming is enabled and the register STREAM_MODE contains a value different than 0, the address pointer loops back to the starting address after the specified number of bytes, allowing continuously writing a register or a block of registers in an indefinitely long SPI frame. This mode is used for waveform playback with minimum overhead.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.