Post Go back to editing

About latency if we do not use each internal blocks (PREMOD, HB1, HB2, HB3, NCO and IQ Modulation)

Category: Hardware
Product Number: AD9148

Hi,

Our customer is considering to operate AD9148 without using internal function blocks.

As the title, how long time delay (= latency) does AD9148 be bypassed each function blocks?

In the datasheet, it has the latency of using function but it does not have value when do not use function.

- Latency of bypassing PREMOD: ??

- Latency of bypassing HB1, 2 and 3: ??

- Latency of bypassing NCO: ??

- Latency of bypassing IQ Modulation: ??

Best Regards,

Kakehi

Parents
  • Hello,

    Latency specs are shown below for the different modes of operation.  Note that 1x interpolation is bypass mode.

  • Hello PMH2023-san,

    Thank you for your reply.

    Please tell me the latency of all functions are same latency?

    For example, 

    PREMOD bypass: 64 cycles

    HB1, 2 and 3 bypass: 64 cycles x 3 = 192 cycles 

    NCO bypass: 64 cycles

    IQ Modulation bypass: 64 cycles

    So, total latency is 64 x 6 = 384 cycles

    Is that correct?

    Best Regards,

    Kakehi

  • Hello,

    With regard to latency specification, it would appear that latency is per function.  Note, the inclusion of course modulation does NOT add to latency due to the manner in which it is implemented (i.e. modify filter coefficient polarity vs actual NCO).  The fine NCO is implemented  with multipliers hence the added 12 cycles.   Also, the pre-mod function does not add to latency since this does not require digital multipliers since data polarity is only being affected (i.e.multiply by +1 or -1).  

    With regard to your example which pertains only to 1x (bypass) mode...........latency is 64 cycles.  If you were to operate in 8x interpolation mode (no inv Sinc or fine mod).............the latency would be 951 cycles (=64+125+254+508) regardless if course modulation via filter was enabled or not.

Reply
  • Hello,

    With regard to latency specification, it would appear that latency is per function.  Note, the inclusion of course modulation does NOT add to latency due to the manner in which it is implemented (i.e. modify filter coefficient polarity vs actual NCO).  The fine NCO is implemented  with multipliers hence the added 12 cycles.   Also, the pre-mod function does not add to latency since this does not require digital multipliers since data polarity is only being affected (i.e.multiply by +1 or -1).  

    With regard to your example which pertains only to 1x (bypass) mode...........latency is 64 cycles.  If you were to operate in 8x interpolation mode (no inv Sinc or fine mod).............the latency would be 951 cycles (=64+125+254+508) regardless if course modulation via filter was enabled or not.

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.