I plan to input 6GHz into the AD9163 CLK, set the DAC clock to 6GSPS, use a data rate of 500MHz, and apply x12 interpolation.
I plan to input a 320MHz signal (-160MHz to +160MHz).
1. It seems to me that there shouldn't be any issues, but are there any potential problems that might prevent this from working?
2. Is it possible to modify the interpolation filter coefficients?
3. Is it possible to use Clock Distribution to lower the 6GHz clock to 2.4GHz, etc.?