Post Go back to editing

DPG-Lite Import complex data

Category: Software
Product Number: 0

In DPG-Lite, there is an option to import arb data from a text file. In the case where I'm using a DAC with complex data generation (ADS9 + AD9081), can the imported vector be complex? Is it just interlaced real and imaginary samples, one per line?

  • Hi  ,

    Thank you for your query. You can import a text file containing the data samples, however I'm not sure if the file can be complex I/Q since that will require two separate data sets. 

    You can try using the Single Tone generator, which can generate a quadrature (complex) tone in addition to the primary (in-phase) tone, by checking the “Generate Complex Data” option. This second (Q) tone is equal in frequency and amplitude to the primary (I) tone but is 90° out of phase.

    By default, the Q tone is -90° relative to the I tone. Entering a negative frequency in the Desired Frequency box will cause the Q tone to be +90°. Using the "Generate Complex Data" option will generate two separate data vectors I and Q on two separate files. 

    Regards,
    Marco

  • Hello. Yes I was aware on generating complex data using the Single Tone, but I'd like to test different/arbitrary waveforms by importing data. It seems strange that there is not a better way to test with complex data to fully test the ad9081 given the price of the ads9...

  • Hi ,


    Good day, you can import an arbitrary data from text file by giving half file as I and half file as Q with a pattern of IIIIQQQQ. Also, please do provide data capture from ACE analysis.

  • @Deferson that sounds reasonable, but there is no checkbox when importing data to indicate complex data vs real dataset. How does the DPG-Lite tool know whether to use the entire file as all-real or the half/half real/complex as you described? 

  • Hi  ,
    DPG-Lite tool will determine thru data formatting if complex or real, depending on the JESD204 mode. For example for mode 15, it is configured as complex.