Is it possible to design a FIR digital filter using FPGA to compensate the amplitude-frequency response of AD9747?
Such as the RZ mode in the figure below.

As shown in Figure AD9854, a digital filter with the opposite response of AD9747 is designed using FPGA to effectively compensate amplitude-frequency distortion.

Assuming that the clock frequency of the AD9747 is 250MHz and the frequency range of the DDS output is 10Hz to 40MHz, how to design a compensation filter in the FPGA?