Post Go back to editing

Circuit for CLOCK input to DAC

Thread Summary

The user asked if the DAC CLK drive circuit is necessary when using ADCLK905 as a clock driver for the AD9783 DAC. The final answer confirmed that the circuit is needed, including 200Ω resistors to bias the LVPECL output stage. The user also inquired about using a fixed crystal oscillator or signal generator as the clock source for the ADCLK905, which is possible but requires the same DAC CLK drive circuit.
AI Generated Content
Category: Datasheet/Specs
Product Number: ad9783

I am having confusion for DAC clock input circuitry as mentioned in datasheet. If suppose I am using ADCLK905 ECL Clock/Data Buffers as Recommended Clock Drivers For low-jitter performance: ADCLK905, ADCLK907, ADCLK925.@ https://www.analog.com/en/products/ad9783.html#product-requirement then should I need additional circuit as mentioned in ad9783 datasheet after the output of ADCLK905 or should I directly feed the output of ADCLK905 to dac ad9783.

so this following circuitry is correct or not?  should I remove DAC CLK drive circuit?