AD9122
Production
The AD9122 is a dual 16-bit, high dynamic range, digital-to-analog converter (DAC) that provides a sample rate of 1230 MSPS, permitting a multicarrier...
Datasheet
AD9122 on Analog.com
ADL5375
Production
The ADL5375 is a broadband quadrature modulator designed for operation from 400 MHz to 6 GHz. Its excellent phase accuracy and amplitude balance enable...
Datasheet
ADL5375 on Analog.com
Hi,
Can AD9122 + ADL5375 generate single test tone with the internal NCO of DAC and how to configure the relevant register ?
That is to say using AD9122 generate the single tone without the data from fpga(D0 to D16).
Thank you !