Post Go back to editing

Glitch Impulse of AD9117

Thread Summary

The user is comparing the AD9707 and AD9117 DACs, specifically regarding their glitch impulse. The AD9707 has a glitch impulse of 5 pV-s, while the AD9117 does not specify this parameter. The MAX5874, with a 1 pV-s glitch impulse, is obsolete. The MAX5891 is suggested as an alternative, offering better settling time and glitch performance, though its INL/DNL at 14-bit level should be verified for the user's digitally controlled servo application.
AI Generated Content
Category: Datasheet/Specs
Product Number: ad9117

Is there a spec / data on the glitch impulse for the AD9117. In my application, I'm deciding between the AD9707 and the AD9117 and I'd like to know the difference in the glitch impulse between the two ADCs. The AD9707  spec's a glitch impulse of 5pV-s. 

Thanks,