Post Go back to editing

how to generate 100MHz sine wave

Category: Hardware
Product Number: 0

1,how to generate 100MHz arbitrary wave;

2,the relation between DAC SPS and DAC max data input rate

  • ADI North America will be on winter shutdown starting December 25, 2023; perhaps another community member can assist you until our return on January 8, 2024.
  • Hi  ,

    1. Not all devices can generate an arbitrary wave. The most reliable way to know if this feature is available is checking if the chip has internal memory. An example of this is the AD9106 which has an internal SRAM for arbitrary waveform generation. 

    2. The relation between the DAC sampling rate and the input data rate depends per device. In most devices, the relation is the Interpolation factor. There is provision for 2x, 4x, and 8x interpolation for most of the devices.

    May I know what product are you referring to? 

    Regards,
    Marco