Post Go back to editing

Settling Time MAX5875

Category: Hardware
Product Number: MAX5875

Hello,

we are using the MAX5875 as a high speed and high accuracy DAC. But we have problems to meet our requirements because of a fairly long settling time.

After a step of the output, the voltage rises within a couple of nanoseconds. But it overshoots the desired value by approximately 9mV (at 5V full scale output) and then it takes hundreds of microseconds to slowly decrease and reach the final value. Strange thing: This error seems to be independant of the step size - whether you step full range or just 100mV, there is always this 9 mV overshoot.

All supply and reference voltages are stable and do not show any change during the step of the DAC values. Do you have an idea what could be the reason for this behaviour?

The schematic of the output:

Full Scale Range is 20 mA and REFIO is an external 1.2V reference voltage source.

red and yellow: Analog output signal zoomed in:

Analog Output zoomed out:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.