Post Go back to editing

AD9176 Balun Output Power Simulation S4P-File as in AN-2065

Category: Datasheet/Specs
Product Number: AD9176

I would like to simulate the output power of the DAC AD9176 in order to analyze the performance of different baluns.

For the DACs of the AD9081, a Keysight ADS model is described in AN-2065 which enables the simulation of the output power.
In this model, an S4P file is supplied which models the output characteristics of the DACs:

As mentioned in this reply, it should be possible to simulate the output power for the AD917x series as well.

Sadly, for the AD917x-series DACs, only S2P-files seem to be available in the .zip-file from the product page:

Are there S4P files available for the AD9176 which can be used to model the output power characteristics?

Thank you very much in advance!

Parents
  • FormerMember
    +2 FormerMember
on Nov 8, 2023 10:14 AM

Hello,

The 4-port model that can be used for the AD917x family of RFDACs was sent to your email address on file.
  
Regards

  • Reply Children
    No Data