Post Go back to editing

AD9142 : Interpolation Configuration

Thread Summary

The user inquired about bypassing the interpolation blocks in the AD9142 DAC to operate in 1x mode. The support engineer confirmed that 1x interpolation is not supported in the AD9142/A, but suggested using the AD9139, which supports 1x and 2x interpolation and has a similar architecture. The block diagram will be revised to clarify this limitation.
AI Generated Content
Product Number: AD9142/AD9142A

Hi,

We are using the AD9142 DAC and trying to bypass the interpolation block in some use cases, the block diagram in the datasheet shows the three 2x interpolation blocks and a bypass path for each. This suggests that it is possible to bypass the interpolation blocks and operate in 1x mode where no FIR are applied to the signal. However, the SPI Interpolation Control Register seems to specify only the 2x, 4x, x8 interpolation modes.

How can we configure the DAC to bypass the interpolation?

Thanks

  • Hi  ,

    We'll look into this and get back to you. 

    Regards,

    Marco

  • Hi  ,

    We've confirmed with one of the designers that 1x interpolation was not released for AD9142/A. If you need to bypass the interpolation filters for your application, there is the AD9139 which has 1x and 2x interpolation. It has a similar architecture to AD9142A and can run at the same max speed, with just a few differences (e.g. no course and fine modulation, no block for input signal power detection and protection, etc.)

    The block diagram was originally illustrated that way because we sometimes allow for HB1 or HB2 to be used individually for 2x (so the switch around HB1 would make sense), however upon testing there were no power or speed savings by letting HB2 be the 2x mode filter option, so it was limited to HB1. We will line this up for datasheet revision.

    Regards,

    Marco

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.