Post Go back to editing

Requirement High Speed DAC

Category: Hardware

Hi Team,

Im new to the design of ADC for 4-20mA analog Input and industrial applications. I have attached the complete design requirement.
Could you please have a look on my attached requirement sheet and share the below Inputs.

1) Suggest ADC part number for below spec?

Number of channels:1 channel (1 channel or 4 channel in a single chip)
Resolution: 16 bit/14bit
Sample rate : 125Msps
Digital Input interface: SPI
Analog Output specification: 4-20mA galvanically isolated output

2)If galvanic isolated DAC is not available, what the galvanic isolated front end circuit can be used? Is there any galvanic isolated amplifier?

Parents Reply Children