Post Go back to editing

Write, Read and generate waveform with SRAM od AD9106

Thread Summary

The user is facing issues with writing and reading data to the SRAM of the AD9106 device and generating a ramp waveform. The final answer indicates that the issue is a duplicate of another thread, suggesting the user refer to the detailed discussion in the linked thread for a solution. The accompanying answer mentions that Analog Devices will be on summer shutdown from August 24 to September 5, 2023, and encourages community assistance in the meantime.
AI Generated Content
Category: Software
Product Number: AD9106

I am reaching out to seek assistance regarding some challenges I am facing with the write and read operations on the SRAM of the AD9106 devices and for generating waveform using sram. I have thoroughly studied the respective datasheets (AD9106 datasheet, pages 22-23) and also Evaluating the AD9106/AD9102 Digital-to-Analog and Waveform Generator Converter using MBED [Analog Devices Wiki] but have encountered difficulties in achieving the desired functionality.

Specifically, I am experiencing issues with:

1) Writing data to the SRAM: For writing data to the SRAM select PAT_STATUS REGISTER 1E=0X04 WRITE Mode. And write data on SRAM Adderess 6000-6FFF as per code example of  AD910x - Library files for EVAL-AD910x | Mbed.

attach code file below 

/*
 * DAC.c
 *
 *  Created on: Jul 26, 2023
 *      Author: Dipak patil
 */

#include "main.h"
#include <stdio.h>
extern void delay_us (uint16_t us);
extern SPI_HandleTypeDef hspi4;
extern UART_HandleTypeDef huart2;


//void DAC(void)
//{
//							// that address and value present in sram section of dac9106 datasheet
//	/*OG*/	                   uint16_t addr[]={0x0000,0x0001,0x0002,0x0003,0x0004,0x0005,0x0006,0x0007,0x0008,0x0009,0x000A,0x000B,0x000C,0x000D,0x000E,0x001F,0x0020,0x0022,0x0023,0x0024,0x0025,0x0026,0x0027,0x0028,0x0029,0x002A,0x002B,0x002C,0x002D,0x002E,0x002F,0x0030,0x0031,0x0032,0x0033,0x0034,0x0035,0x0036,0x0037,0x003E,0x003F,0x0040,0x0041,0x0042,0x0043,0x0044,0x0045,0x0046,0x0047,0x0050,0x0051,0x0052,0x0053,0x0054,0x0055,0x0056,0x0057,0x0058,0x0059,0x005A,0x005B,0x005C,0x005D,0x005E,0x005F,0x0060,0x001D,0x001E};
//							   uint16_t Valu[]={0x0000,0x0E00,0x0000,0x0000,0x4000,0x4000,0x4000,0x4000,0x0000,0x1F00,0x1F00,0x1F00,0x1F00,0x0000,0x0000,0x0000,0x000E,0x0000,0x0000,0x0000,0x0000,0x1212,0x1232,0x0111,0x6D60,0x0101,0x0101,0x0003,0x0000,0x0000,0x0000,0x0000,0x0000,0x4000,0x4000,0x4000,0x4000,0x1011,0x1010,0x002B,0xB100,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x07D0,0x0000,0x0000,0x0001,0x03E8,0x0000,0x0000,0x0100,0x0BB8,0x0000,0xFFF0,0x0100,0x0FA0,0x0000,0xFFF0,0x0100,0x0005,0x0001,0x0001};
///*sine og*/                 // uint16_t Valu[]={0x0000,0x0E00,0x0000,0x0000,0x4000,0x4000,0x4000,0x4000,0x0000,0x1F00,0x1F00,0x1F00,0x1F00,0x0000,0x0000,0x0000,0x000E,0x0000,0x0000,0x0000,0x0000,0x3232,0x3232,0x0111,0xFFFF,0x0101,0x0101,0x0003,0x0000,0x0000,0x0000,0x0000,0x0000,0x4000,0x4000/*AMPLITUTE*/,0x4000,0x4000,0x0001,0x0200,0x06D3/*MSB*/,0xA100/*LSB*/,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x07D0,0x0000,0x0000,0x0100,0x0100,0x0000,0x0000,0x0100,0x0BB8,0x0000,0x0000,0x0100,0x0FA0,0x0000,0x0000,0x0100,0x0004,0x0001,0x0001};
///*Sawtooth varible freq og*/ //uint16_t Valu[]={0x0000,0x0E00,0x0000,0x0000,0x4000,0x4000,0x4000,0x4000,0x0000,0x1F00,0x1F00,0x1F00,0x1F00,0x0000,0x0000,0x0000,0x000E,0x0000,0x0000,0x0000,0x0000,0x1212,0x1231,0x0111,0x61A8,0x0101,0x0101,0x0003,0x0000,0x0000,0x0000,0x0000,0x0000,0x4000,0x4000,0x4000,0x4000,0x1010,0x0600,0x0036,0x9D00,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x07D0,0x0000,0x0000,0x0001,0x03E8,0x0000,0x0000,0x0100,0x03E8,0x0000,0x0000,0x0001,0x0FA0,0x0000,0x0000,0x16FF,0x0004,0x0001,0x0001};
///*ramp up sawtooth//og*/ //    uint16_t Valu[]={0x0000,0x0E00,0x0000,0x0000,0x4000,0x4000,0x4000,0x4000,0x0000,0x1F00,0x1F00,0x1F00,0x1F00,0x0000,0x0000,0x0000,0x000E,0x0000,0x0000,0x0000,0x0000,0x1212,0x1232,0x0111,0xFFFF,0x0101,0x0101,0x0003,0x0000,0x0000,0x0000,0x0000,0x0000,0x4000,0x4000,0x4000,0x4000,0x1010,0x0600,0x0036,0x9D00,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x07D0,0x0000,0x0000,0x0001,0x03E8,0x0000,0x0000,0x0100,0x03E8,0x0000,0x0000,0x0001,0x0FA0,0x0000,0x0000,0x16FF,0x0004,0x0001,0x0001};
///*ramp dawn sawtooth//og*/  //   uint16_t Valu[]={0x0000,0x0E00,0x0000,0x0000,0x4000,0x4000,0x4000,0x4000,0x0000,0x1F00,0x1F00,0x1F00,0x1F00,0x0000,0x0000,0x0000,0x000E,0x0000,0x0000,0x0000,0x0000,0x1212,0x1232,0x0111,0xFFFF,0x0101,0x0101,0x0003,0x0000,0x0000,0x0000,0x0000,0x0000,0x4000,0x4000,0x4000,0x4000,0x1011,0x0600,0x0036,0x9D00,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x07D0,0x0000,0x0000,0x0001,0x03E8,0x0000,0x0000,0x0100,0x03E8,0x0000,0x0000,0x0001,0x0FA0,0x0000,0x0000,0x16FF,0x0004,0x0001,0x0001};
//
//				/*og */        uint16_t Radd[]={0x8000,0x8001,0x8002,0x8003,0x8004,0x8005,0x8006,0x8007,0x8008,0x8009,0x800A,0x800B,0x800C,0x000D,0x000E,0x801F,0x8020,0x8022,0x8023,0x8024,0x8025,0x8026,0x8027,0x8028,0x8029,0x802A,0x802B,0x802C,0x802D,0x802E,0x802F,0x8030,0x8031,0x8032,0x8033,0x8034,0x8035,0x8036,0x8037,0x803E,0x803F,0x8040,0x8041,0x8042,0x8043,0x8044,0x8045,0x8046,0x8047,0x8050,0x8051,0x8052,0x8053,0x8054,0x8055,0x8056,0x8057,0x8058,0x8059,0x805A,0x805B,0x805C,0x805D,0x805E,0x805F,0x8060,0x001D,0x001E};
//             	 	 	 	 	 //                0        1      2     3      4      5        6    7      8      9      10     11     12      13    14     15      16     17     18    19     20      21   22      23    24       25     26    27     28        29     30   31     32     33    34     35     36     37      38    39      40     41    42      43    44     45      46     47    48     49        50    51    52     53   54      55       56    57      58    59   60       61      62     63    64  65        66     67
//
////////////////////////////////////////////////////////////////
////comment out for the pre-store values waveform
////
//
//	int i=0,j=0,k=0;
//	uint16_t Read_Value=0;
//	uint8_t s=0,s1=0,s2=0,s3=0;
//
//	for(i=0,j=0,k=0;i<69;i++,j++,k++) //////////////////////////67
//	{
//		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);  // Activate CS
//		s=HAL_SPI_Transmit(&hspi4, (uint8_t*)&addr[i], 1, 100);    // spi transmit address to dac ad9106 one by one
//		s1=HAL_SPI_Transmit(&hspi4,(uint8_t*)&Valu[j], 1, 100);		// spi transmit value to dac ad9106 one by one
//		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);	// Deactivate CS
//		printf("3s=%d s=%d W- A=%x, V=%x\n\r",s,s1,addr[i],Valu[j]); // check transmitted address/value and declare address/value same or not
//		delay_us(10);
////		HAL_Delay(100);
//
//		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);    // Activate CS
//		s2=HAL_SPI_Transmit(&hspi4, (uint8_t*)&Radd[k], 1, 100);		// spi transmit read address
//		s3=HAL_SPI_Receive(&hspi4,(uint8_t*)&Read_Value,1, 100);		// spi receive value for check read value right or not
//		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);		// Deactivate CS
//		printf("4s=%d s=%d R- A=%x,V=%x\n\n\r",s2,s3,Radd[k],Read_Value);
//		delay_us(10);
////		HAL_Delay(100);
//
////	}
//	HAL_GPIO_WritePin(GPIOH,Trigger1_Pin, GPIO_PIN_RESET);   /////////////////remove comment for sawtooth
//	delay_us(5000);
////	HAL_Delay(5000);
//	HAL_GPIO_WritePin(GPIOH,Trigger1_Pin, GPIO_PIN_SET);
//	}
//////////////////////////////////////////////////////////////////////////////////////
//
//}



void SRAM_DAC(void)
{
			uint16_t reg_addr[]={0x0000, 0x0001, 0x0002, 0x0003, 0x0004, 0x0005, 0x0006, 0x0007, 0x0008, 0x0009, 0x000a, 0x000b, 0x000c, 0x000d, 0x000e, 0x001f, 0x0020, 0x0022, 0x0023, 0x0024, 0x0025, 0x0026, 0x0027, 0x0028, 0x0029, 0x002a, 0x002b, 0x002c, 0x002d, 0x002e, 0x002f, 0x0030, 0x0031, 0x0032, 0x0033, 0x0034, 0x0035, 0x0036, 0x0037, 0x003e, 0x003f, 0x0040, 0x0041, 0x0042, 0x0043, 0x0044, 0x0045, 0x0047, 0x0050, 0x0051, 0x0052, 0x0053, 0x0054, 0x0055, 0x0056, 0x0057, 0x0058, 0x0059, 0x005a, 0x005b, 0x005c, 0x005d, 0x005e, 0x005f, 0x001e, 0x001d};

   uint16_t sramramp_regval[66]={0x0000, 0x0e00, 0x0000, 0x0000, 0x4000, 0x4000, 0x4000, 0x4000, 0x0000, 0x1f00, 0x1f00, 0x1f00, 0x1f00, 0x0000, 0x0000, 0x0000, 0x000e, 0x0000, 0x0000, 0x0000, 0x0000, 0x3030, 0x3030, 0x0111, 0xffff, 0x0101, 0x0101, 0x0003, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x4000, 0x2000, 0x2000, 0x4000, 0x0001, 0x0200, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x07d0, 0xc000, 0xfff0, 0x0100, 0x03e8, 0x8000, 0xbff0, 0x0100, 0x0bb8, 0x3ff0, 0x7ff0, 0x0100, 0x0fa0, 0x0000, 0x3ff0, 0x0100, 0x0001, 0x0001};
   int16_t sram_ramp[4096]={-2048, -2047, -2046, -2045, -2044, -2043, -2042, -2041, -2040, -2039, -2038, -2037, -2036, -2035, -2034, -2033, -2032, -2031, -2030, -2029, -2028, -2027, -2026, -2025, -2024, -2023, -2022, -2021, -2020, -2019, -2018, -2017, -2016, -2015, -2014, -2013, -2012, -2011, -2010, -2009, -2008, -2007, -2006, -2005, -2004, -2003, -2002, -2001, -2000, -1999, -1998, -1997, -1996, -1995, -1994, -1993, -1992, -1991, -1990, -1989, -1988, -1987, -1986, -1985, -1984, -1983, -1982, -1981, -1980, -1979, -1978, -1977, -1976, -1975, -1974, -1973, -1972, -1971, -1970, -1969, -1968, -1967, -1966, -1965, -1964, -1963, -1962, -1961, -1960, -1959, -1958, -1957, -1956, -1955, -1954, -1953, -1952, -1951, -1950, -1949, -1948, -1947, -1946, -1945, -1944, -1943, -1942, -1941, -1940, -1939, -1938, -1937, -1936, -1935, -1934, -1933, -1932, -1931, -1930, -1929, -1928, -1927, -1926, -1925, -1924, -1923, -1922, -1921, -1920, -1919, -1918, -1917, -1916, -1915, -1914, -1913, -1912, -1911, -1910, -1909, -1908, -1907, -1906, -1905, -1904, -1903, -1902, -1901, -1900, -1899, -1898, -1897, -1896, -1895, -1894, -1893, -1892, -1891, -1890, -1889, -1888, -1887, -1886, -1885, -1884, -1883, -1882, -1881, -1880, -1879, -1878, -1877, -1876, -1875, -1874, -1873, -1872, -1871, -1870, -1869, -1868, -1867, -1866, -1865, -1864, -1863, -1862, -1861, -1860, -1859, -1858, -1857, -1856, -1855, -1854, -1853, -1852, -1851, -1850, -1849, -1848, -1847, -1846, -1845, -1844, -1843, -1842, -1841, -1840, -1839, -1838, -1837, -1836, -1835, -1834, -1833, -1832, -1831, -1830, -1829, -1828, -1827, -1826, -1825, -1824, -1823, -1822, -1821, -1820, -1819, -1818, -1817, -1816, -1815, -1814, -1813, -1812, -1811, -1810, -1809, -1808, -1807, -1806, -1805, -1804, -1803, -1802, -1801, -1800, -1799, -1798, -1797, -1796, -1795, -1794, -1793, -1792, -1791, -1790, -1789, -1788, -1787, -1786, -1785, -1784, -1783, -1782, -1781, -1780, -1779, -1778, -1777, -1776, -1775, -1774, -1773, -1772, -1771, -1770, -1769, -1768, -1767, -1766, -1765, -1764, -1763, -1762, -1761, -1760, -1759, -1758, -1757, -1756, -1755, -1754, -1753, -1752, -1751, -1750, -1749, -1748, -1747, -1746, -1745, -1744, -1743, -1742, -1741, -1740, -1739, -1738, -1737, -1736, -1735, -1734, -1733, -1732, -1731, -1730, -1729, -1728, -1727, -1726, -1725, -1724, -1723, -1722, -1721, -1720, -1719, -1718, -1717, -1716, -1715, -1714, -1713, -1712, -1711, -1710, -1709, -1708, -1707, -1706, -1705, -1704, -1703, -1702, -1701, -1700, -1699, -1698, -1697, -1696, -1695, -1694, -1693, -1692, -1691, -1690, -1689, -1688, -1687, -1686, -1685, -1684, -1683, -1682, -1681, -1680, -1679, -1678, -1677, -1676, -1675, -1674, -1673, -1672, -1671, -1670, -1669, -1668, -1667, -1666, -1665, -1664, -1663, -1662, -1661, -1660, -1659, -1658, -1657, -1656, -1655, -1654, -1653, -1652, -1651, -1650, -1649, -1648, -1647, -1646, -1645, -1644, -1643, -1642, -1641, -1640, -1639, -1638, -1637, -1636, -1635, -1634, -1633, -1632, -1631, -1630, -1629, -1628, -1627, -1626, -1625, -1624, -1623, -1622, -1621, -1620, -1619, -1618, -1617, -1616, -1615, -1614, -1613, -1612, -1611, -1610, -1609, -1608, -1607, -1606, -1605, -1604, -1603, -1602, -1601, -1600, -1599, -1598, -1597, -1596, -1595, -1594, -1593, -1592, -1591, -1590, -1589, -1588, -1587, -1586, -1585, -1584, -1583, -1582, -1581, -1580, -1579, -1578, -1577, -1576, -1575, -1574, -1573, -1572, -1571, -1570, -1569, -1568, -1567, -1566, -1565, -1564, -1563, -1562, -1561, -1560, -1559, -1558, -1557, -1556, -1555, -1554, -1553, -1552, -1551, -1550, -1549, -1548, -1547, -1546, -1545, -1544, -1543, -1542, -1541, -1540, -1539, -1538, -1537, -1536, -1535, -1534, -1533, -1532, -1531, -1530, -1529, -1528, -1527, -1526, -1525, -1524, -1523, -1522, -1521, -1520, -1519, -1518, -1517, -1516, -1515, -1514, -1513, -1512, -1511, -1510, -1509, -1508, -1507, -1506, -1505, -1504, -1503, -1502, -1501, -1500, -1499, -1498, -1497, -1496, -1495, -1494, -1493, -1492, -1491, -1490, -1489, -1488, -1487, -1486, -1485, -1484, -1483, -1482, -1481, -1480, -1479, -1478, -1477, -1476, -1475, -1474, -1473, -1472, -1471, -1470, -1469, -1468, -1467, -1466, -1465, -1464, -1463, -1462, -1461, -1460, -1459, -1458, -1457, -1456, -1455, -1454, -1453, -1452, -1451, -1450, -1449, -1448, -1447, -1446, -1445, -1444, -1443, -1442, -1441, -1440, -1439, -1438, -1437, -1436, -1435, -1434, -1433, -1432, -1431, -1430, -1429, -1428, -1427, -1426, -1425, -1424, -1423, -1422, -1421, -1420, -1419, -1418, -1417, -1416, -1415, -1414, -1413, -1412, -1411, -1410, -1409, -1408, -1407, -1406, -1405, -1404, -1403, -1402, -1401, -1400, -1399, -1398, -1397, -1396, -1395, -1394, -1393, -1392, -1391, -1390, -1389, -1388, -1387, -1386, -1385, -1384, -1383, -1382, -1381, -1380, -1379, -1378, -1377, -1376, -1375, -1374, -1373, -1372, -1371, -1370, -1369, -1368, -1367, -1366, -1365, -1364, -1363, -1362, -1361, -1360, -1359, -1358, -1357, -1356, -1355, -1354, -1353, -1352, -1351, -1350, -1349, -1348, -1347, -1346, -1345, -1344, -1343, -1342, -1341, -1340, -1339, -1338, -1337, -1336, -1335, -1334, -1333, -1332, -1331, -1330, -1329, -1328, -1327, -1326, -1325, -1324, -1323, -1322, -1321, -1320, -1319, -1318, -1317, -1316, -1315, -1314, -1313, -1312, -1311, -1310, -1309, -1308, -1307, -1306, -1305, -1304, -1303, -1302, -1301, -1300, -1299, -1298, -1297, -1296, -1295, -1294, -1293, -1292, -1291, -1290, -1289, -1288, -1287, -1286, -1285, -1284, -1283, -1282, -1281, -1280, -1279, -1278, -1277, -1276, -1275, -1274, -1273, -1272, -1271, -1270, -1269, -1268, -1267, -1266, -1265, -1264, -1263, -1262, -1261, -1260, -1259, -1258, -1257, -1256, -1255, -1254, -1253, -1252, -1251, -1250, -1249, -1248, -1247, -1246, -1245, -1244, -1243, -1242, -1241, -1240, -1239, -1238, -1237, -1236, -1235, -1234, -1233, -1232, -1231, -1230, -1229, -1228, -1227, -1226, -1225, -1224, -1223, -1222, -1221, -1220, -1219, -1218, -1217, -1216, -1215, -1214, -1213, -1212, -1211, -1210, -1209, -1208, -1207, -1206, -1205, -1204, -1203, -1202, -1201, -1200, -1199, -1198, -1197, -1196, -1195, -1194, -1193, -1192, -1191, -1190, -1189, -1188, -1187, -1186, -1185, -1184, -1183, -1182, -1181, -1180, -1179, -1178, -1177, -1176, -1175, -1174, -1173, -1172, -1171, -1170, -1169, -1168, -1167, -1166, -1165, -1164, -1163, -1162, -1161, -1160, -1159, -1158, -1157, -1156, -1155, -1154, -1153, -1152, -1151, -1150, -1149, -1148, -1147, -1146, -1145, -1144, -1143, -1142, -1141, -1140, -1139, -1138, -1137, -1136, -1135, -1134, -1133, -1132, -1131, -1130, -1129, -1128, -1127, -1126, -1125, -1124, -1123, -1122, -1121, -1120, -1119, -1118, -1117, -1116, -1115, -1114, -1113, -1112, -1111, -1110, -1109, -1108, -1107, -1106, -1105, -1104, -1103, -1102, -1101, -1100, -1099, -1098, -1097, -1096, -1095, -1094, -1093, -1092, -1091, -1090, -1089, -1088, -1087, -1086, -1085, -1084, -1083, -1082, -1081, -1080, -1079, -1078, -1077, -1076, -1075, -1074, -1073, -1072, -1071, -1070, -1069, -1068, -1067, -1066, -1065, -1064, -1063, -1062, -1061, -1060, -1059, -1058, -1057, -1056, -1055, -1054, -1053, -1052, -1051, -1050, -1049, -1048, -1047, -1046, -1045, -1044, -1043, -1042, -1041, -1040, -1039, -1038, -1037, -1036, -1035, -1034, -1033, -1032, -1031, -1030, -1029, -1028, -1027, -1026, -1025, -1024, -1023, -1022, -1021, -1020, -1019, -1018, -1017, -1016, -1015, -1014, -1013, -1012, -1011, -1010, -1009, -1008, -1007, -1006, -1005, -1004, -1003, -1002, -1001, -1000, -999, -998, -997, -996, -995, -994, -993, -992, -991, -990, -989, -988, -987, -986, -985, -984, -983, -982, -981, -980, -979, -978, -977, -976, -975, -974, -973, -972, -971, -970, -969, -968, -967, -966, -965, -964, -963, -962, -961, -960, -959, -958, -957, -956, -955, -954, -953, -952, -951, -950, -949, -948, -947, -946, -945, -944, -943, -942, -941, -940, -939, -938, -937, -936, -935, -934, -933, -932, -931, -930, -929, -928, -927, -926, -925, -924, -923, -922, -921, -920, -919, -918, -917, -916, -915, -914, -913, -912, -911, -910, -909, -908, -907, -906, -905, -904, -903, -902, -901, -900, -899, -898, -897, -896, -895, -894, -893, -892, -891, -890, -889, -888, -887, -886, -885, -884, -883, -882, -881, -880, -879, -878, -877, -876, -875, -874, -873, -872, -871, -870, -869, -868, -867, -866, -865, -864, -863, -862, -861, -860, -859, -858, -857, -856, -855, -854, -853, -852, -851, -850, -849, -848, -847, -846, -845, -844, -843, -842, -841, -840, -839, -838, -837, -836, -835, -834, -833, -832, -831, -830, -829, -828, -827, -826, -825, -824, -823, -822, -821, -820, -819, -818, -817, -816, -815, -814, -813, -812, -811, -810, -809, -808, -807, -806, -805, -804, -803, -802, -801, -800, -799, -798, -797, -796, -795, -794, -793, -792, -791, -790, -789, -788, -787, -786, -785, -784, -783, -782, -781, -780, -779, -778, -777, -776, -775, -774, -773, -772, -771, -770, -769, -768, -767, -766, -765, -764, -763, -762, -761, -760, -759, -758, -757, -756, -755, -754, -753, -752, -751, -750, -749, -748, -747, -746, -745, -744, -743, -742, -741, -740, -739, -738, -737, -736, -735, -734, -733, -732, -731, -730, -729, -728, -727, -726, -725, -724, -723, -722, -721, -720, -719, -718, -717, -716, -715, -714, -713, -712, -711, -710, -709, -708, -707, -706, -705, -704, -703, -702, -701, -700, -699, -698, -697, -696, -695, -694, -693, -692, -691, -690, -689, -688, -687, -686, -685, -684, -683, -682, -681, -680, -679, -678, -677, -676, -675, -674, -673, -672, -671, -670, -669, -668, -667, -666, -665, -664, -663, -662, -661, -660, -659, -658, -657, -656, -655, -654, -653, -652, -651, -650, -649, -648, -647, -646, -645, -644, -643, -642, -641, -640, -639, -638, -637, -636, -635, -634, -633, -632, -631, -630, -629, -628, -627, -626, -625, -624, -623, -622, -621, -620, -619, -618, -617, -616, -615, -614, -613, -612, -611, -610, -609, -608, -607, -606, -605, -604, -603, -602, -601, -600, -599, -598, -597, -596, -595, -594, -593, -592, -591, -590, -589, -588, -587, -586, -585, -584, -583, -582, -581, -580, -579, -578, -577, -576, -575, -574, -573, -572, -571, -570, -569, -568, -567, -566, -565, -564, -563, -562, -561, -560, -559, -558, -557, -556, -555, -554, -553, -552, -551, -550, -549, -548, -547, -546, -545, -544, -543, -542, -541, -540, -539, -538, -537, -536, -535, -534, -533, -532, -531, -530, -529, -528, -527, -526, -525, -524, -523, -522, -521, -520, -519, -518, -517, -516, -515, -514, -513, -512, -511, -510, -509, -508, -507, -506, -505, -504, -503, -502, -501, -500, -499, -498, -497, -496, -495, -494, -493, -492, -491, -490, -489, -488, -487, -486, -485, -484, -483, -482, -481, -480, -479, -478, -477, -476, -475, -474, -473, -472, -471, -470, -469, -468, -467, -466, -465, -464, -463, -462, -461, -460, -459, -458, -457, -456, -455, -454, -453, -452, -451, -450, -449, -448, -447, -446, -445, -444, -443, -442, -441, -440, -439, -438, -437, -436, -435, -434, -433, -432, -431, -430, -429, -428, -427, -426, -425, -424, -423, -422, -421, -420, -419, -418, -417, -416, -415, -414, -413, -412, -411, -410, -409, -408, -407, -406, -405, -404, -403, -402, -401, -400, -399, -398, -397, -396, -395, -394, -393, -392, -391, -390, -389, -388, -387, -386, -385, -384, -383, -382, -381, -380, -379, -378, -377, -376, -375, -374, -373, -372, -371, -370, -369, -368, -367, -366, -365, -364, -363, -362, -361, -360, -359, -358, -357, -356, -355, -354, -353, -352, -351, -350, -349, -348, -347, -346, -345, -344, -343, -342, -341, -340, -339, -338, -337, -336, -335, -334, -333, -332, -331, -330, -329, -328, -327, -326, -325, -324, -323, -322, -321, -320, -319, -318, -317, -316, -315, -314, -313, -312, -311, -310, -309, -308, -307, -306, -305, -304, -303, -302, -301, -300, -299, -298, -297, -296, -295, -294, -293, -292, -291, -290, -289, -288, -287, -286, -285, -284, -283, -282, -281, -280, -279, -278, -277, -276, -275, -274, -273, -272, -271, -270, -269, -268, -267, -266, -265, -264, -263, -262, -261, -260, -259, -258, -257, -256, -255, -254, -253, -252, -251, -250, -249, -248, -247, -246, -245, -244, -243, -242, -241, -240, -239, -238, -237, -236, -235, -234, -233, -232, -231, -230, -229, -228, -227, -226, -225, -224, -223, -222, -221, -220, -219, -218, -217, -216, -215, -214, -213, -212, -211, -210, -209, -208, -207, -206, -205, -204, -203, -202, -201, -200, -199, -198, -197, -196, -195, -194, -193, -192, -191, -190, -189, -188, -187, -186, -185, -184, -183, -182, -181, -180, -179, -178, -177, -176, -175, -174, -173, -172, -171, -170, -169, -168, -167, -166, -165, -164, -163, -162, -161, -160, -159, -158, -157, -156, -155, -154, -153, -152, -151, -150, -149, -148, -147, -146, -145, -144, -143, -142, -141, -140, -139, -138, -137, -136, -135, -134, -133, -132, -131, -130, -129, -128, -127, -126, -125, -124, -123, -122, -121, -120, -119, -118, -117, -116, -115, -114, -113, -112, -111, -110, -109, -108, -107, -106, -105, -104, -103, -102, -101, -100, -99, -98, -97, -96, -95, -94, -93, -92, -91, -90, -89, -88, -87, -86, -85, -84, -83, -82, -81, -80, -79, -78, -77, -76, -75, -74, -73, -72, -71, -70, -69, -68, -67, -66, -65, -64, -63, -62, -61, -60, -59, -58, -57, -56, -55, -54, -53, -52, -51, -50, -49, -48, -47, -46, -45, -44, -43, -42, -41, -40, -39, -38, -37, -36, -35, -34, -33, -32, -31, -30, -29, -28, -27, -26, -25, -24, -23, -22, -21, -20, -19, -18, -17, -16, -15, -14, -13, -12, -11, -10, -9, -8, -7, -6, -5, -4, -3, -2, -1, 0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 16, 17, 18, 19, 20, 21, 22, 23, 24, 25, 26, 27, 28, 29, 30, 31, 32, 33, 34, 35, 36, 37, 38, 39, 40, 41, 42, 43, 44, 45, 46, 47, 48, 49, 50, 51, 52, 53, 54, 55, 56, 57, 58, 59, 60, 61, 62, 63, 64, 65, 66, 67, 68, 69, 70, 71, 72, 73, 74, 75, 76, 77, 78, 79, 80, 81, 82, 83, 84, 85, 86, 87, 88, 89, 90, 91, 92, 93, 94, 95, 96, 97, 98, 99, 100, 101, 102, 103, 104, 105, 106, 107, 108, 109, 110, 111, 112, 113, 114, 115, 116, 117, 118, 119, 120, 121, 122, 123, 124, 125, 126, 127, 128, 129, 130, 131, 132, 133, 134, 135, 136, 137, 138, 139, 140, 141, 142, 143, 144, 145, 146, 147, 148, 149, 150, 151, 152, 153, 154, 155, 156, 157, 158, 159, 160, 161, 162, 163, 164, 165, 166, 167, 168, 169, 170, 171, 172, 173, 174, 175, 176, 177, 178, 179, 180, 181, 182, 183, 184, 185, 186, 187, 188, 189, 190, 191, 192, 193, 194, 195, 196, 197, 198, 199, 200, 201, 202, 203, 204, 205, 206, 207, 208, 209, 210, 211, 212, 213, 214, 215, 216, 217, 218, 219, 220, 221, 222, 223, 224, 225, 226, 227, 228, 229, 230, 231, 232, 233, 234, 235, 236, 237, 238, 239, 240, 241, 242, 243, 244, 245, 246, 247, 248, 249, 250, 251, 252, 253, 254, 255, 256, 257, 258, 259, 260, 261, 262, 263, 264, 265, 266, 267, 268, 269, 270, 271, 272, 273, 274, 275, 276, 277, 278, 279, 280, 281, 282, 283, 284, 285, 286, 287, 288, 289, 290, 291, 292, 293, 294, 295, 296, 297, 298, 299, 300, 301, 302, 303, 304, 305, 306, 307, 308, 309, 310, 311, 312, 313, 314, 315, 316, 317, 318, 319, 320, 321, 322, 323, 324, 325, 326, 327, 328, 329, 330, 331, 332, 333, 334, 335, 336, 337, 338, 339, 340, 341, 342, 343, 344, 345, 346, 347, 348, 349, 350, 351, 352, 353, 354, 355, 356, 357, 358, 359, 360, 361, 362, 363, 364, 365, 366, 367, 368, 369, 370, 371, 372, 373, 374, 375, 376, 377, 378, 379, 380, 381, 382, 383, 384, 385, 386, 387, 388, 389, 390, 391, 392, 393, 394, 395, 396, 397, 398, 399, 400, 401, 402, 403, 404, 405, 406, 407, 408, 409, 410, 411, 412, 413, 414, 415, 416, 417, 418, 419, 420, 421, 422, 423, 424, 425, 426, 427, 428, 429, 430, 431, 432, 433, 434, 435, 436, 437, 438, 439, 440, 441, 442, 443, 444, 445, 446, 447, 448, 449, 450, 451, 452, 453, 454, 455, 456, 457, 458, 459, 460, 461, 462, 463, 464, 465, 466, 467, 468, 469, 470, 471, 472, 473, 474, 475, 476, 477, 478, 479, 480, 481, 482, 483, 484, 485, 486, 487, 488, 489, 490, 491, 492, 493, 494, 495, 496, 497, 498, 499, 500, 501, 502, 503, 504, 505, 506, 507, 508, 509, 510, 511, 512, 513, 514, 515, 516, 517, 518, 519, 520, 521, 522, 523, 524, 525, 526, 527, 528, 529, 530, 531, 532, 533, 534, 535, 536, 537, 538, 539, 540, 541, 542, 543, 544, 545, 546, 547, 548, 549, 550, 551, 552, 553, 554, 555, 556, 557, 558, 559, 560, 561, 562, 563, 564, 565, 566, 567, 568, 569, 570, 571, 572, 573, 574, 575, 576, 577, 578, 579, 580, 581, 582, 583, 584, 585, 586, 587, 588, 589, 590, 591, 592, 593, 594, 595, 596, 597, 598, 599, 600, 601, 602, 603, 604, 605, 606, 607, 608, 609, 610, 611, 612, 613, 614, 615, 616, 617, 618, 619, 620, 621, 622, 623, 624, 625, 626, 627, 628, 629, 630, 631, 632, 633, 634, 635, 636, 637, 638, 639, 640, 641, 642, 643, 644, 645, 646, 647, 648, 649, 650, 651, 652, 653, 654, 655, 656, 657, 658, 659, 660, 661, 662, 663, 664, 665, 666, 667, 668, 669, 670, 671, 672, 673, 674, 675, 676, 677, 678, 679, 680, 681, 682, 683, 684, 685, 686, 687, 688, 689, 690, 691, 692, 693, 694, 695, 696, 697, 698, 699, 700, 701, 702, 703, 704, 705, 706, 707, 708, 709, 710, 711, 712, 713, 714, 715, 716, 717, 718, 719, 720, 721, 722, 723, 724, 725, 726, 727, 728, 729, 730, 731, 732, 733, 734, 735, 736, 737, 738, 739, 740, 741, 742, 743, 744, 745, 746, 747, 748, 749, 750, 751, 752, 753, 754, 755, 756, 757, 758, 759, 760, 761, 762, 763, 764, 765, 766, 767, 768, 769, 770, 771, 772, 773, 774, 775, 776, 777, 778, 779, 780, 781, 782, 783, 784, 785, 786, 787, 788, 789, 790, 791, 792, 793, 794, 795, 796, 797, 798, 799, 800, 801, 802, 803, 804, 805, 806, 807, 808, 809, 810, 811, 812, 813, 814, 815, 816, 817, 818, 819, 820, 821, 822, 823, 824, 825, 826, 827, 828, 829, 830, 831, 832, 833, 834, 835, 836, 837, 838, 839, 840, 841, 842, 843, 844, 845, 846, 847, 848, 849, 850, 851, 852, 853, 854, 855, 856, 857, 858, 859, 860, 861, 862, 863, 864, 865, 866, 867, 868, 869, 870, 871, 872, 873, 874, 875, 876, 877, 878, 879, 880, 881, 882, 883, 884, 885, 886, 887, 888, 889, 890, 891, 892, 893, 894, 895, 896, 897, 898, 899, 900, 901, 902, 903, 904, 905, 906, 907, 908, 909, 910, 911, 912, 913, 914, 915, 916, 917, 918, 919, 920, 921, 922, 923, 924, 925, 926, 927, 928, 929, 930, 931, 932, 933, 934, 935, 936, 937, 938, 939, 940, 941, 942, 943, 944, 945, 946, 947, 948, 949, 950, 951, 952, 953, 954, 955, 956, 957, 958, 959, 960, 961, 962, 963, 964, 965, 966, 967, 968, 969, 970, 971, 972, 973, 974, 975, 976, 977, 978, 979, 980, 981, 982, 983, 984, 985, 986, 987, 988, 989, 990, 991, 992, 993, 994, 995, 996, 997, 998, 999, 1000, 1001, 1002, 1003, 1004, 1005, 1006, 1007, 1008, 1009, 1010, 1011, 1012, 1013, 1014, 1015, 1016, 1017, 1018, 1019, 1020, 1021, 1022, 1023, 1024, 1025, 1026, 1027, 1028, 1029, 1030, 1031, 1032, 1033, 1034, 1035, 1036, 1037, 1038, 1039, 1040, 1041, 1042, 1043, 1044, 1045, 1046, 1047, 1048, 1049, 1050, 1051, 1052, 1053, 1054, 1055, 1056, 1057, 1058, 1059, 1060, 1061, 1062, 1063, 1064, 1065, 1066, 1067, 1068, 1069, 1070, 1071, 1072, 1073, 1074, 1075, 1076, 1077, 1078, 1079, 1080, 1081, 1082, 1083, 1084, 1085, 1086, 1087, 1088, 1089, 1090, 1091, 1092, 1093, 1094, 1095, 1096, 1097, 1098, 1099, 1100, 1101, 1102, 1103, 1104, 1105, 1106, 1107, 1108, 1109, 1110, 1111, 1112, 1113, 1114, 1115, 1116, 1117, 1118, 1119, 1120, 1121, 1122, 1123, 1124, 1125, 1126, 1127, 1128, 1129, 1130, 1131, 1132, 1133, 1134, 1135, 1136, 1137, 1138, 1139, 1140, 1141, 1142, 1143, 1144, 1145, 1146, 1147, 1148, 1149, 1150, 1151, 1152, 1153, 1154, 1155, 1156, 1157, 1158, 1159, 1160, 1161, 1162, 1163, 1164, 1165, 1166, 1167, 1168, 1169, 1170, 1171, 1172, 1173, 1174, 1175, 1176, 1177, 1178, 1179, 1180, 1181, 1182, 1183, 1184, 1185, 1186, 1187, 1188, 1189, 1190, 1191, 1192, 1193, 1194, 1195, 1196, 1197, 1198, 1199, 1200, 1201, 1202, 1203, 1204, 1205, 1206, 1207, 1208, 1209, 1210, 1211, 1212, 1213, 1214, 1215, 1216, 1217, 1218, 1219, 1220, 1221, 1222, 1223, 1224, 1225, 1226, 1227, 1228, 1229, 1230, 1231, 1232, 1233, 1234, 1235, 1236, 1237, 1238, 1239, 1240, 1241, 1242, 1243, 1244, 1245, 1246, 1247, 1248, 1249, 1250, 1251, 1252, 1253, 1254, 1255, 1256, 1257, 1258, 1259, 1260, 1261, 1262, 1263, 1264, 1265, 1266, 1267, 1268, 1269, 1270, 1271, 1272, 1273, 1274, 1275, 1276, 1277, 1278, 1279, 1280, 1281, 1282, 1283, 1284, 1285, 1286, 1287, 1288, 1289, 1290, 1291, 1292, 1293, 1294, 1295, 1296, 1297, 1298, 1299, 1300, 1301, 1302, 1303, 1304, 1305, 1306, 1307, 1308, 1309, 1310, 1311, 1312, 1313, 1314, 1315, 1316, 1317, 1318, 1319, 1320, 1321, 1322, 1323, 1324, 1325, 1326, 1327, 1328, 1329, 1330, 1331, 1332, 1333, 1334, 1335, 1336, 1337, 1338, 1339, 1340, 1341, 1342, 1343, 1344, 1345, 1346, 1347, 1348, 1349, 1350, 1351, 1352, 1353, 1354, 1355, 1356, 1357, 1358, 1359, 1360, 1361, 1362, 1363, 1364, 1365, 1366, 1367, 1368, 1369, 1370, 1371, 1372, 1373, 1374, 1375, 1376, 1377, 1378, 1379, 1380, 1381, 1382, 1383, 1384, 1385, 1386, 1387, 1388, 1389, 1390, 1391, 1392, 1393, 1394, 1395, 1396, 1397, 1398, 1399, 1400, 1401, 1402, 1403, 1404, 1405, 1406, 1407, 1408, 1409, 1410, 1411, 1412, 1413, 1414, 1415, 1416, 1417, 1418, 1419, 1420, 1421, 1422, 1423, 1424, 1425, 1426, 1427, 1428, 1429, 1430, 1431, 1432, 1433, 1434, 1435, 1436, 1437, 1438, 1439, 1440, 1441, 1442, 1443, 1444, 1445, 1446, 1447, 1448, 1449, 1450, 1451, 1452, 1453, 1454, 1455, 1456, 1457, 1458, 1459, 1460, 1461, 1462, 1463, 1464, 1465, 1466, 1467, 1468, 1469, 1470, 1471, 1472, 1473, 1474, 1475, 1476, 1477, 1478, 1479, 1480, 1481, 1482, 1483, 1484, 1485, 1486, 1487, 1488, 1489, 1490, 1491, 1492, 1493, 1494, 1495, 1496, 1497, 1498, 1499, 1500, 1501, 1502, 1503, 1504, 1505, 1506, 1507, 1508, 1509, 1510, 1511, 1512, 1513, 1514, 1515, 1516, 1517, 1518, 1519, 1520, 1521, 1522, 1523, 1524, 1525, 1526, 1527, 1528, 1529, 1530, 1531, 1532, 1533, 1534, 1535, 1536, 1537, 1538, 1539, 1540, 1541, 1542, 1543, 1544, 1545, 1546, 1547, 1548, 1549, 1550, 1551, 1552, 1553, 1554, 1555, 1556, 1557, 1558, 1559, 1560, 1561, 1562, 1563, 1564, 1565, 1566, 1567, 1568, 1569, 1570, 1571, 1572, 1573, 1574, 1575, 1576, 1577, 1578, 1579, 1580, 1581, 1582, 1583, 1584, 1585, 1586, 1587, 1588, 1589, 1590, 1591, 1592, 1593, 1594, 1595, 1596, 1597, 1598, 1599, 1600, 1601, 1602, 1603, 1604, 1605, 1606, 1607, 1608, 1609, 1610, 1611, 1612, 1613, 1614, 1615, 1616, 1617, 1618, 1619, 1620, 1621, 1622, 1623, 1624, 1625, 1626, 1627, 1628, 1629, 1630, 1631, 1632, 1633, 1634, 1635, 1636, 1637, 1638, 1639, 1640, 1641, 1642, 1643, 1644, 1645, 1646, 1647, 1648, 1649, 1650, 1651, 1652, 1653, 1654, 1655, 1656, 1657, 1658, 1659, 1660, 1661, 1662, 1663, 1664, 1665, 1666, 1667, 1668, 1669, 1670, 1671, 1672, 1673, 1674, 1675, 1676, 1677, 1678, 1679, 1680, 1681, 1682, 1683, 1684, 1685, 1686, 1687, 1688, 1689, 1690, 1691, 1692, 1693, 1694, 1695, 1696, 1697, 1698, 1699, 1700, 1701, 1702, 1703, 1704, 1705, 1706, 1707, 1708, 1709, 1710, 1711, 1712, 1713, 1714, 1715, 1716, 1717, 1718, 1719, 1720, 1721, 1722, 1723, 1724, 1725, 1726, 1727, 1728, 1729, 1730, 1731, 1732, 1733, 1734, 1735, 1736, 1737, 1738, 1739, 1740, 1741, 1742, 1743, 1744, 1745, 1746, 1747, 1748, 1749, 1750, 1751, 1752, 1753, 1754, 1755, 1756, 1757, 1758, 1759, 1760, 1761, 1762, 1763, 1764, 1765, 1766, 1767, 1768, 1769, 1770, 1771, 1772, 1773, 1774, 1775, 1776, 1777, 1778, 1779, 1780, 1781, 1782, 1783, 1784, 1785, 1786, 1787, 1788, 1789, 1790, 1791, 1792, 1793, 1794, 1795, 1796, 1797, 1798, 1799, 1800, 1801, 1802, 1803, 1804, 1805, 1806, 1807, 1808, 1809, 1810, 1811, 1812, 1813, 1814, 1815, 1816, 1817, 1818, 1819, 1820, 1821, 1822, 1823, 1824, 1825, 1826, 1827, 1828, 1829, 1830, 1831, 1832, 1833, 1834, 1835, 1836, 1837, 1838, 1839, 1840, 1841, 1842, 1843, 1844, 1845, 1846, 1847, 1848, 1849, 1850, 1851, 1852, 1853, 1854, 1855, 1856, 1857, 1858, 1859, 1860, 1861, 1862, 1863, 1864, 1865, 1866, 1867, 1868, 1869, 1870, 1871, 1872, 1873, 1874, 1875, 1876, 1877, 1878, 1879, 1880, 1881, 1882, 1883, 1884, 1885, 1886, 1887, 1888, 1889, 1890, 1891, 1892, 1893, 1894, 1895, 1896, 1897, 1898, 1899, 1900, 1901, 1902, 1903, 1904, 1905, 1906, 1907, 1908, 1909, 1910, 1911, 1912, 1913, 1914, 1915, 1916, 1917, 1918, 1919, 1920, 1921, 1922, 1923, 1924, 1925, 1926, 1927, 1928, 1929, 1930, 1931, 1932, 1933, 1934, 1935, 1936, 1937, 1938, 1939, 1940, 1941, 1942, 1943, 1944, 1945, 1946, 1947, 1948, 1949, 1950, 1951, 1952, 1953, 1954, 1955, 1956, 1957, 1958, 1959, 1960, 1961, 1962, 1963, 1964, 1965, 1966, 1967, 1968, 1969, 1970, 1971, 1972, 1973, 1974, 1975, 1976, 1977, 1978, 1979, 1980, 1981, 1982, 1983, 1984, 1985, 1986, 1987, 1988, 1989, 1990, 1991, 1992, 1993, 1994, 1995, 1996, 1997, 1998, 1999, 2000, 2001, 2002, 2003, 2004, 2005, 2006, 2007, 2008, 2009, 2010, 2011, 2012, 2013, 2014, 2015, 2016, 2017, 2018, 2019, 2020, 2021, 2022, 2023, 2024, 2025, 2026, 2027, 2028, 2029, 2030, 2031, 2032, 2033, 2034, 2035, 2036, 2037, 2038, 2039, 2040, 2041, 2042, 2043, 2044, 2045, 2046, 2047};

	//		uint16_t ddssine_regval[66]={0x0000, 0x0e00, 0x0000, 0x0000, 0x4000, 0x4000, 0x4000, 0x4000, 0x0000, 0x1f00, 0x1f00, 0x1f00, 0x1f00, 0x0000, 0x0000, 0x0000, 0x000e, 0x0000, 0x0000, 0x0000, 0x0000, 0x3232, 0x3232, 0x0111, 0xffff, 0x0101, 0x0101, 0x0003, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x4000, 0x4000, 0x4000, 0x4000, 0x0001, 0x0200, 0x0a3d, 0x7100, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x07d0, 0x0000, 0x0000, 0x0100, 0x03e8, 0x0000, 0x0000, 0x0100, 0x0bb8, 0x0000, 0x0000, 0x0100, 0x0fa0, 0x0000, 0x0000, 0x0100, 0x0001, 0x0001};

//
//    uint16_t gaussian_regval[]={0x0000, 0x0e00, 0x0000, 0x0000, 0x4000, 0x4000, 0x4000, 0x4000, 0x0000, 0x1f00, 0x1f00, 0x1f00, 0x1f00, 0x0000, 0x0000, 0x0000, 0x000e, 0x0000, 0x0000, 0x0000, 0x0000, 0x3333, 0x3333, 0x0111, 0xffff, 0x0101, 0x0101, 0x0003, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x4000, 0x4000, 0x4000, 0x4000, 0x0001, 0x0200, 0x0750, 0x7500, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x07d0, 0x0000, 0xfff0, 0x0100, 0x03e8, 0x0000, 0xfff0, 0x0100, 0x0bb8, 0x0000, 0xfff0, 0x0100, 0x0fa0, 0x0000, 0xfff0, 0x0100, 0x0001, 0x0001};
//			int16_t sram_gaussian[4096]={0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 4, 4, 4, 4, 4, 4, 4, 4, 4, 4, 4, 5, 5, 5, 5, 5, 5, 5, 5, 5, 6, 6, 6, 6, 6, 6, 6, 6, 7, 7, 7, 7, 7, 7, 7, 8, 8, 8, 8, 8, 9, 9, 9, 9, 9, 9, 10, 10, 10, 10, 10, 11, 11, 11, 11, 12, 12, 12, 12, 13, 13, 13, 13, 14, 14, 14, 15, 15, 15, 16, 16, 16, 17, 17, 17, 18, 18, 18, 19, 19, 20, 20, 20, 21, 21, 22, 22, 23, 23, 23, 24, 24, 25, 25, 26, 27, 27, 28, 28, 29, 29, 30, 31, 31, 32, 33, 33, 34, 35, 35, 36, 37, 37, 38, 39, 40, 41, 41, 42, 43, 44, 45, 46, 47, 48, 49, 50, 51, 52, 53, 54, 55, 56, 57, 58, 60, 61, 62, 63, 65, 66, 67, 69, 70, 72, 73, 75, 76, 78, 79, 81, 82, 84, 86, 88, 89, 91, 93, 95, 97, 99, 101, 103, 105, 107, 109, 111, 114, 116, 118, 121, 123, 126, 128, 131, 133, 136, 139, 142, 145, 148, 151, 154, 157, 160, 163, 166, 170, 173, 177, 180, 184, 188, 192, 195, 199, 203, 207, 212, 216, 220, 225, 229, 234, 239, 244, 249, 254, 259, 264, 269, 275, 280, 286, 292, 298, 304, 310, 316, 322, 329, 336, 342, 349, 356, 364, 371, 378, 386, 394, 402, 410, 418, 427, 435, 444, 453, 462, 472, 481, 491, 501, 511, 521, 532, 543, 554, 565, 576, 588, 600, 612, 624, 637, 650, 663, 676, 690, 704, 718, 733, 748, 763, 778, 794, 810, 826, 843, 860, 877, 895, 913, 932, 951, 970, 989, 1009, 1030, 1051, 1072, 1093, 1116, 1138, 1161, 1185, 1208, 1233, 1258, 1283, 1309, 1336, 1363, 1390, 1418, 1447, 1476, 1506, 1536, 1567, 1599, 1631, 1664, 1698, 1732, 1767, 1803, 1840, 1877, 1915, 1953, 1993, 2033, 2074, 2116, 2159, 2202, 2247, 2292, 2339, 2386, 2434, 2483, 2533, 2585, 2637, 2690, 2744, 2800, 2856, 2914, 2973, 3033, 3094, 3157, 3221, 3286, 3352, 3420, 3489, 3560, 3631, 3705, 3780, 3856, 3934, 4013, 4095, 4013, 3934, 3856, 3780, 3705, 3631, 3560, 3489, 3420, 3352, 3286, 3221, 3157, 3094, 3033, 2973, 2914, 2856, 2800, 2744, 2690, 2637, 2585, 2533, 2483, 2434, 2386, 2339, 2292, 2247, 2202, 2159, 2116, 2074, 2033, 1993, 1953, 1915, 1877, 1840, 1803, 1767, 1732, 1698, 1664, 1631, 1599, 1567, 1536, 1506, 1476, 1447, 1418, 1390, 1363, 1336, 1309, 1283, 1258, 1233, 1208, 1185, 1161, 1138, 1116, 1093, 1072, 1051, 1030, 1009, 989, 970, 951, 932, 913, 895, 877, 860, 843, 826, 810, 794, 778, 763, 748, 733, 718, 704, 690, 676, 663, 650, 637, 624, 612, 600, 588, 576, 565, 554, 543, 532, 521, 511, 501, 491, 481, 472, 462, 453, 444, 435, 427, 418, 410, 402, 394, 386, 378, 371, 364, 356, 349, 342, 336, 329, 322, 316, 310, 304, 298, 292, 286, 280, 275, 269, 264, 259, 254, 249, 244, 239, 234, 229, 225, 220, 216, 212, 207, 203, 199, 195, 192, 188, 184, 180, 177, 173, 170, 166, 163, 160, 157, 154, 151, 148, 145, 142, 139, 136, 133, 131, 128, 126, 123, 121, 118, 116, 114, 111, 109, 107, 105, 103, 101, 99, 97, 95, 93, 91, 89, 88, 86, 84, 82, 81, 79, 78, 76, 75, 73, 72, 70, 69, 67, 66, 65, 63, 62, 61, 60, 58, 57, 56, 55, 54, 53, 52, 51, 50, 49, 48, 47, 46, 45, 44, 43, 42, 41, 41, 40, 39, 38, 37, 37, 36, 35, 35, 34, 33, 33, 32, 31, 31, 30, 29, 29, 28, 28, 27, 27, 26, 25, 25, 24, 24, 23, 23, 23, 22, 22, 21, 21, 20, 20, 20, 19, 19, 18, 18, 18, 17, 17, 17, 16, 16, 16, 15, 15, 15, 14, 14, 14, 13, 13, 13, 13, 12, 12, 12, 12, 11, 11, 11, 11, 10, 10, 10, 10, 10, 9, 9, 9, 9, 9, 9, 8, 8, 8, 8, 8, 7, 7, 7, 7, 7, 7, 7, 6, 6, 6, 6, 6, 6, 6, 6, 5, 5, 5, 5, 5, 5, 5, 5, 5, 4, 4, 4, 4, 4, 4, 4, 4, 4, 4, 4, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0};

				printf("*******SRAM*******\n\r");

				update_sram(sram_ramp);
				update_regs( reg_addr,sramramp_regval);

//				update_sram(sram_gaussian);
//				update_regs( reg_addr,gaussian_regval);

		// update_regs( reg_addr,ddssine_regval );   //dds sine wave   working

				 start_pattern();


}

void update_sram( int16_t sram_ramp_data[] )
{

//	uint16_t s=0,s1=0,s2=0,s3=0,s4=0,s6=0;
//	int16_t s5=0,s7=0;

///////////////////////////////////sram write mode
	sram_write();
	//HAL_Delay(1000);
///////////////////////////////////sram store value
	uint16_t sram_add=0x6000;

	int16_t sram_datashiftleft = 0;
	for(int i=0;i<4096;i++){
		uint16_t s4=0;
			int16_t s5=0;
		int16_t sram_datashiftleft = sram_ramp_data[i] << 4;

		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);  // Activate CS
		s4=HAL_SPI_Transmit(&hspi4, (uint16_t*)&sram_add+i, sizeof(sram_add+i), 100);    // spi transmit sram address to dac ad9106 one by one
		s5=HAL_SPI_Transmit(&hspi4, (int16_t*)&sram_datashiftleft, sizeof(sram_datashiftleft), 100);    // spi transmit address to dac ad9106 one by one
		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);	// Deactivate CS
		printf("3s=%d s=%d sram_reg_addr=%x, sram_reg_value=%x\n\r",s4,s5,sram_add+i,sram_datashiftleft); // check transmitted address/value and declare address/value same or not
		delay_us(50);
//		HAL_Delay(100);

//		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);    // Activate CS
//		s6=HAL_SPI_Transmit(&hspi4, (uint16_t*)&read_sram_addr, 1, 100);		// spi transmit read address
//		s7=HAL_SPI_Receive(&hspi4,(int16_t*)&Read_sram_Value,1, 100);		// spi receive value for check read value right or not
//		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);		// Deactivate CS
//		printf("4s=%d s=%d read_sram_addr=%x,read_sram_value=%d\n\n\r",s6,s7,read_sram_addr,Read_sram_Value);
//		delay_us(10);
////		HAL_Delay(100);

//		HAL_GPIO_WritePin(GPIOH, Trigger1_Pin, GPIO_PIN_RESET);
//		delay_us(1000);
//			//HAL_Delay(10000);
//		HAL_GPIO_WritePin(GPIOH, Trigger1_Pin, GPIO_PIN_SET);
		}
	//HAL_Delay(1000);

///////////////////////////////sram mode PAT=0X0000
	reg_clear();
	//HAL_Delay(1000);
////////////////

//////////////////////////////sram read mode
		sram_read();
		//HAL_Delay(1000);

/////////////////////////////////////sram read store value
		       int16_t Read_sram_Value=0;
			  int16_t sram_datashiftright = 0;
				for(int j=0;j<4096;j++){
					uint16_t s6=0;
					int16_t s7=0;
					uint16_t read_sram_addr = 0x8000+sram_add+j;
				//	uint16_t read_sram_addr = sram_add+j;

					HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);    // Activate CS
					s6=HAL_SPI_Transmit(&hspi4, (uint16_t*)&read_sram_addr, sizeof(read_sram_addr), 100);		// spi transmit read address
					delay_us(100);
					s7=HAL_SPI_Receive(&hspi4,(int16_t*)&Read_sram_Value,sizeof(Read_sram_Value), 100);		// spi receive value for check read value right or not
					delay_us(100);
				//	Read_sram_Value=HAL_SPI_Transmit(&hspi4, 0, 1, 100);		// spi transmit read address
				//	delay_us(100);
					HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);		// Deactivate CS
					sram_datashiftright = Read_sram_Value >> 4;
					printf("4s=%d s=%d read_sram_addr=%x,read_sram_value=%x\n\n\r",s6,s7,read_sram_addr,sram_datashiftright);
					delay_us(50);
			//		HAL_Delay(100);

//					HAL_GPIO_WritePin(GPIOH, Trigger1_Pin, GPIO_PIN_RESET);
//					delay_us(1000);
//						//HAL_Delay(10000);
//					HAL_GPIO_WritePin(GPIOH, Trigger1_Pin, GPIO_PIN_SET);
					}
	//	HAL_Delay(1000);

///////////////////////////////////////sram mode
				reg_clear();
			//	HAL_Delay(1000);


}

void update_regs(uint16_t reg_addr[],uint16_t regval[] ){

	//       uint16_t Radd[]={0x8000,0x8001,0x8002,0x8003,0x8004,0x8005,0x8006,0x8007,0x8008,0x8009,0x800A,0x800B,0x800C,0x000D,0x000E,0x801F,0x8020,0x8022,0x8023,0x8024,0x8025,0x8026,0x8027,0x8028,0x8029,0x802A,0x802B,0x802C,0x802D,0x802E,0x802F,0x8030,0x8031,0x8032,0x8033,0x8034,0x8035,0x8036,0x8037,0x803E,0x803F,0x8040,0x8041,0x8042,0x8043,0x8044,0x8045,0x8047,0x8050,0x8051,0x8052,0x8053,0x8054,0x8055,0x8056,0x8057,0x8058,0x8059,0x805A,0x805B,0x805C,0x805D,0x805E,0x805F,0x001E,0x001D};
	         //                0        1      2     3      4      5        6    7      8      9      10     11     12      13    14     15      16     17     18    19     20      21   22      23    24       25     26    27     28        29     30   31     32     33    34     35     36     37      38    39      40     41    42      43    44     45      46     47    48     49        50    51    52     53   54      55       56    57      58    59   60       61      62     63    64  65        66     67

	int i=0,j=0,k=0;
		uint16_t Read_Value=0;
		uint16_t s=0,s1=0,s2=0,s3=0;

		for(i=0,j=0;i<66;i++,j++) //////////////////////////67
		{
			uint16_t read_addr = 0x8000+reg_addr[i];
			HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);  // Activate CS
			s=HAL_SPI_Transmit(&hspi4, (uint16_t*)&reg_addr[i], 1, 100);    // spi transmit address to dac ad9106 one by one
			s1=HAL_SPI_Transmit(&hspi4,(uint16_t*)&regval[j], 1, 100);		// spi transmit value to dac ad9106 one by one
			HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);	// Deactivate CS
			printf("3s=%d s=%d reg_addr=%x, reg_addr_value=%x\n\r",s,s1,reg_addr[i],regval[j]); // check transmitted address/value and declare address/value same or not
			delay_us(50);
	//		HAL_Delay(100);

			HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);    // Activate CS
		//	s2=HAL_SPI_Transmit(&hspi4, (uint16_t*)&Radd[k], 1, 100);		// spi transmit read address
			s2=HAL_SPI_Transmit(&hspi4, (uint16_t*)&read_addr, 1, 100);		// spi transmit read address
			s3=HAL_SPI_Receive(&hspi4,(uint16_t*)&Read_Value,1, 100);		// spi receive value for check read value right or not
			HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);		// Deactivate CS
		//	printf("4s=%d s=%d R- A=%x,V=%x\n\n\r",s2,s3,Radd[k],Read_Value);
			printf("4s=%d s=%d read_reg_addr=%x,read_reg_addr_value=%x\n\n\r",s2,s3,read_addr,Read_Value);
			delay_us(50);
	//		HAL_Delay(100);

//		HAL_GPIO_WritePin(GPIOH,Trigger1_Pin, GPIO_PIN_RESET);   /////////////////remove comment for sawtooth
//		delay_us(1000);
//	//	HAL_Delay(5000);
//		HAL_GPIO_WritePin(GPIOH,Trigger1_Pin, GPIO_PIN_SET);
		}
	//	HAL_Delay(10000);
}
void sram_write(void){
	uint16_t s=0,s1=0,s2=0,s3=0;

	  uint16_t reg_addr=0x001E,valu=0x04;       //PAT_status reg for write=0x0004
		  uint16_t Radd_PAT=0x801E;
		   uint16_t Read_Value=0;
		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);    // Activate CS
		s=HAL_SPI_Transmit(&hspi4, (uint16_t*)&reg_addr, 1, 100);			// load address of PAT_Status_Reg
		s1=HAL_SPI_Transmit(&hspi4,(uint16_t*)&valu, 1, 100);			// load value in PAT Status reg run bit high
		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);    // Deactivate CS
		printf("1s=%d s=%d PAT_reg_addr=%x, PAT_reg_value=%x\n\r",s,s1,reg_addr,valu);
		delay_us(500);
	//		HAL_Delay(500);

		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);
		s2=HAL_SPI_Transmit(&hspi4, (uint16_t*)&Radd_PAT, 1, 100);
		s3=HAL_SPI_Receive(&hspi4,(uint16_t*)&Read_Value,1, 100);
		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);
		printf("2s=%d s=%d Radd_PAT=%x,Radd_PAT_Value=%x\n\n\r",s2,s3,Radd_PAT,Read_Value);
		delay_us(500);
	//		HAL_Delay(500);
//		HAL_GPIO_WritePin(GPIOH, Trigger1_Pin, GPIO_PIN_RESET);
//		delay_us(1000);
//		//	HAL_Delay(10000);
//		HAL_GPIO_WritePin(GPIOH, Trigger1_Pin, GPIO_PIN_SET);
//	//	HAL_Delay(10000);
}

void sram_read(void){
	uint16_t s=0,s1=0,s2=0,s3=0;
	uint16_t reg_addr=0x001E,valu=0x000C;       //PAT_status reg for read=0x000c
	uint16_t Radd_PAT=0x801E;
	uint16_t Read_Value=0;
		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);    // Activate CS
		s=HAL_SPI_Transmit(&hspi4, (uint16_t*)&reg_addr, 1, 100);			// load address of PAT_Status_Reg
		s1=HAL_SPI_Transmit(&hspi4,(uint16_t*)&valu, 1, 100);			// load value in PAT Status reg run bit high
		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);    // Deactivate CS
		printf("1s=%d s=%d PAT_reg_addr=%x, PAT_reg_value=%x\n\r",s,s1,reg_addr,valu);
		delay_us(50);
	//		HAL_Delay(500);

		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);
		s2=HAL_SPI_Transmit(&hspi4, (uint16_t*)&Radd_PAT, 1, 100);
		s3=HAL_SPI_Receive(&hspi4,(uint16_t*)&Read_Value,1, 100);
		HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);
		printf("2s=%d s=%d Radd_PAT=%x,Radd_PAT_Value=%x\n\n\r",s2,s3,Radd_PAT,Read_Value);
		delay_us(50);
	//		HAL_Delay(500);
//		HAL_GPIO_WritePin(GPIOH, Trigger1_Pin, GPIO_PIN_RESET);
//		delay_us(1000);
//			//HAL_Delay(10000);
//		HAL_GPIO_WritePin(GPIOH, Trigger1_Pin, GPIO_PIN_SET);
//		//HAL_Delay(10000);

}
void reg_clear(void){
	uint16_t s=0,s1=0,s2=0,s3=0;
	uint16_t reg_addr=0x001E,valu=0x10;       //PAT_status reg for END write=0x0000
		uint16_t Radd_PAT=0x801E;
		uint16_t Read_Value=0;
			HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);    // Activate CS
			s=HAL_SPI_Transmit(&hspi4, (uint16_t*)&reg_addr, 1, 100);			// load address of PAT_Status_Reg
			s1=HAL_SPI_Transmit(&hspi4,(uint16_t*)&valu, 1, 100);			// load value in PAT Status reg run bit high
			HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);    // Deactivate CS
			printf("1s=%d s=%d PAT_reg_addr=%x, PAT_reg_value=%x\n\r",s,s1,reg_addr,valu);
			delay_us(50);
		//		HAL_Delay(500);

			HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);
			s2=HAL_SPI_Transmit(&hspi4, (uint16_t*)&Radd_PAT, 1, 100);
			s3=HAL_SPI_Receive(&hspi4,(uint16_t*)&Read_Value,1, 100);
			HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);
			printf("2s=%d s=%d Radd_PAT=%x,Radd_PAT_Value=%x\n\n\r",s2,s3,Radd_PAT,Read_Value);
			delay_us(50);
		//		HAL_Delay(500);
//			HAL_GPIO_WritePin(GPIOH, Trigger1_Pin, GPIO_PIN_RESET);
//			delay_us(1000);
//				//HAL_Delay(10000);
//			HAL_GPIO_WritePin(GPIOH, Trigger1_Pin, GPIO_PIN_SET);
//
//	//		HAL_Delay(1000);

}

void start_pattern(void){

					uint16_t reg_addr=0x001E,valu=0x01;       //PAT_status reg for RUN=0x0001
					uint16_t Radd_PAT=0x801E,Read_Value=0;
					uint16_t s=0,s1=0,s2=0,s3=0;

					HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);    // Activate CS
					s=HAL_SPI_Transmit(&hspi4, (uint16_t*)&reg_addr, 1, 100);			// load address of PAT_Status_Reg
					s1=HAL_SPI_Transmit(&hspi4,(uint16_t*)&valu, 1, 100);			// load value in PAT Status reg run bit high
					HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);    // Deactivate CS
					printf("1s=%d s=%d PAT_reg_addr=%x, PAT_reg_value=%x\n\r",s,s1,reg_addr,valu);
					delay_us(50);
			//		HAL_Delay(500);

					HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_RESET);
					s2=HAL_SPI_Transmit(&hspi4, (uint16_t*)&Radd_PAT, 1, 100);
					s3=HAL_SPI_Receive(&hspi4,(uint16_t*)&Read_Value,1, 100);
					HAL_GPIO_WritePin(CS1_GPIO_Port, CS1_Pin, GPIO_PIN_SET);
					printf("2s=%d s=%d Radd_PAT=%x,Radd_PAT_Value=%x\n\n\r",s2,s3,Radd_PAT,Read_Value);
					delay_us(50);
					HAL_Delay(500);

					HAL_GPIO_WritePin(GPIOH, Trigger1_Pin, GPIO_PIN_RESET);      //start pattern
					delay_us(5000);
						HAL_Delay(10000);
					HAL_GPIO_WritePin(GPIOH, Trigger1_Pin, GPIO_PIN_SET);		 // stop pattern
				//	delay_us(5000);
				//	HAL_Delay(10000);
}

2) Reading data to the SRAM: For writing data to the SRAM select PAT_STATUS REGISTER 1E=0X0C Read Mode. I read data that from SRAM address 0xE000-0xEFFF   That calculate by 8000+starting sram address... as per code example of AD910x - Library files for EVAL-AD910x | Mbed .

but i reading value not same as write value. i attach write value output   

and read value output   

and haven't got expected ramp waveform    

I have thoroughly reviewed the datasheets, but it appears that I may be missing some crucial steps or misinterpreting certain instructions. I would greatly appreciate it if you could provide me with guidance and clarification on the correct procedure for performing write and read operations on the SRAM of the AD9106 devices.

If possible, could you please provide me with detailed step-by-step instructions, highlighting any potential pitfalls or commonly overlooked aspects of the process? Additionally, if there are any specific register settings or considerations I should be aware of, kindly provide those details as well.

I understand that your team has extensive expertise in working with these devices, and I am confident that your guidance will help me overcome the challenges I am currently facing.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.