Post Go back to editing

AD9735 DAC stops working after some time

Thread Summary

The user encountered an issue with the AD9735 DAC where the output signal would disappear after 20-40 minutes, despite the clock and SPI communication remaining functional. The problem was likely due to improper termination of LVDS lines, which was resolved. However, the user now faces periodic 1 GHz spikes in the output signal, even when sending a stable data value. The Analog Devices support engineer suggested checking the output circuitry, clock source, and register configurations, and provided a reference to the DAC output distortion sources and clock input driving sections in the datasheet. The user's current register settings and a schematic of the output circuitry were shared for further analysis.
AI Generated Content
Category: Hardware

Hi, I have a problem with the operation of the AD9735 chip.

We have produced two custom PCBs using these chips. In both there is the same problem. The circuit after switching on works correctly, the signal generated is correct, the circuit reads the configuration, responds, for example, to PD mode, change of current(reg 2,3). However, after some time, usually about 20-40 minutes, the circuit stops working. The output data disappears. The clock is still present, data from the FPGA processor is sent, SPI communication works. The temperature of the chip , measured with a thermocouple-type probe, is about 40 degrees C.

Schematic:

reading registers during correct operation, reading registers after a malfunction:



DAC clocking signal: 500/600 MHz
If the problem occurs, the only solution is to temporarily cut off power to the DAC chip. Simply uploading the configuration, turning PD mode on and off, uploading the FPGA configuration again, does not resume the DAC operation.

Best regards,
MM

Parents
  • Hi MM,

    Your query is acknowledged and will be responded by the product owner soon.

    Best regards,
    Peevee

  • Hello,
    it's been a month since I wrote a request for help. Until now, I haven't heard from anyone. Does Analog Devices provide any technical support for their products? Are users forced to solve all problems on their own?

    During testing I was able to verify that the converter has 3 possible modes of operation into which it enters after a power start:
    1. voltage level VPP A,
    2. voltage level VPP B,
    3. no output signal but with SPI communication operation. 

    All with the same input signal....

Reply
  • Hello,
    it's been a month since I wrote a request for help. Until now, I haven't heard from anyone. Does Analog Devices provide any technical support for their products? Are users forced to solve all problems on their own?

    During testing I was able to verify that the converter has 3 possible modes of operation into which it enters after a power start:
    1. voltage level VPP A,
    2. voltage level VPP B,
    3. no output signal but with SPI communication operation. 

    All with the same input signal....

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.