Post Go back to editing

What's the difference between "Gain drift" and "Gain error drift"?

Thread Summary

The user inquired about the difference between 'offset error drift' and 'gain error drift' in the LTC2000A datasheet and 'offset drift' and 'gain drift' in the AD9136 datasheet. The support engineer confirmed that these terms refer to the same parameters, which measure variations in offset and gain due to temperature changes. The performance of temperature drift cannot be directly compared between the two devices due to different evaluation conditions: AD9136 is evaluated from -40°C to +85°C, while LTC2000A is evaluated at +25°C.
AI Generated Content
Category: Datasheet/Specs
Product Number: LTC2000A, AD9136

The paramter of temperature drift in LTC2000A‘s datasheet is named "offset error drift" and "Gain error drift". Howerver, this relative parameter is named "gain drift" and "offset drift" without "error" in AD9136's datasheet. Are they the same?If not, what's the difference and which chip's performance of temperature drift is better? Thanks.

Paramter of temperature drift in LTC2000A's datasheet

Paramter of temperature drift in AD9136's datasheet

  • Hi  ,

    I believe those terms pertain to the same thing. In the AD9136 Datasheet, these terms are under the "Temperature Drift" terminology. Offset Drift and Gain Drift are variations in offset error/gain error due to a change in ambient temperature, and both are typically expressed in ppm of full-scale range (FSR) per °C (ppm/°C). 

    Regarding performance, the two cannot be compared directly because the temperature drift specs for both devices were evaluated at different conditions: AD9136 temperature drifts is evaluated at ambient operating temperature of -40°C to +85°C, while LTC2000A is at evaluated at +25°C.

    Regards,

    Marco

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.