Post Go back to editing

FPGA source code for Device DA9177 ? Could you share with me ?

AD9177 API config.

Parents Reply Children
  • Both the AD9081 and the AD9082 have 4 dacs, which is the same as the AD9177. The difference is the number of ADCs (9081 has 4 adcs, 9082 has 2, and 9177 has none). If you have a 9177 evaluation board you can use ACE with the ad9081 plugin to configure, or you can request the 9177 api code to view/edit the startup in more detail. All the dacs in these chip families have the same architecture and are programmed the same way.