Does the AD9739 have a similar delay function as the AD9744,as shown in the figure below. When changing the clock delay, IOUT is delayed with the delay of the clock. If not, Is there a way to change the delay of IOUT,thx
AD9739
Production
The AD9739 is a 14-bit, 2.5 GSPS high performance RF digital-to-analog converter (DAC) capable of synthesizing wideband
signals from dc up to 3.0 GHz....
Datasheet
AD9739 on Analog.com
AD9744
Production
The AD97441 is a 14-bit resolution, wideband, third generation member of the TxDAC series of high performance, low power CMOS digital-to-analog converters...
Datasheet
AD9744 on Analog.com
Does the AD9739 have a similar delay function as the AD9744,as shown in the figure below. When changing the clock delay, IOUT is delayed with the delay of the clock. If not, Is there a way to change the delay of IOUT,thx