hi all:
I'm a beginner in DACs.I have a question in AD9136.
In the example of AD9136 rev.D P79. As shown below.
We can known SERDES lanes run at 7.3728 Gbps.
(1)And the fref of SERDES PLL is 1/40 of the lane rate. That is 184.32MHz. As shown below in P37.
(2)In P38, the fref is equal to BIT RATE÷40. And we can get the fref from the equations in P37. ByteRate is 184.32MHz. And BIT RATE is 23.04MHz. So the fref is 0.576MHz. (I think the BIT RATE is ByteRate?)
(3)In P4, the fref of SERDES PLL is DACCLK.But DACCLK is 1474.56MHz in the above example. Is there some correlation between fref and DACCLK?
So,I'm confused about fref of SERDES PLL. And Which of the above is correct?
Best Regards