In datasheet, output of ad9739 is connected to TC1-33-75G2+, using 90Ω to GND in figure 65. Now,i want to amplify the amplitude of output, can i use bigger resistor here, i.e, 100Ω,150Ω?
AD9739
Production
The AD9739 is a 14-bit, 2.5 GSPS high performance RF digital-to-analog converter (DAC) capable of synthesizing wideband
signals from dc up to 3.0 GHz....
Datasheet
AD9739 on Analog.com
In datasheet, output of ad9739 is connected to TC1-33-75G2+, using 90Ω to GND in figure 65. Now,i want to amplify the amplitude of output, can i use bigger resistor here, i.e, 100Ω,150Ω?
Hi licunxu,
Your query is acknowledged and will be responded by the product owner soon.
Regards,
Peevee
Hi, is there a reply by the product owner
Hi Licunxu,
thanks for the question. I don't recommend changing the 90ohm. (70ohm // (90+90)ohm ) = 50ohm, this is the impedance driving by the DAC for an optimal match.
If you like to amplify the signal, you could use Figure 67 with RF differential amp
what type of application is that?
Thanks
Adam