Hello,
I am using AD9139 for the transmitter, the evaluation board uses two buluns, why use two balun? What's the effect of using only one? Thanks!
AD9139
Recommended for New Designs
The AD9139 is a 16-bit, high dynamic range digital-to-analog
converter (DAC) that provides a maximum update rate of 1600 MSPS,
permitting multicarrier...
Datasheet
AD9139 on Analog.com
Hello,
I am using AD9139 for the transmitter, the evaluation board uses two buluns, why use two balun? What's the effect of using only one? Thanks!
Hi Draogn ,
The two baluns in the DAC output data paths are for converting the differential output to single ended while suppressing the noise coming from the feedline (the 1:1 balun acts as an isolator). If using only one balun (i.e. the 1:2 balun only), SNR may not be optimal due to noise.
Regards,
Marco
Hi Draogn ,
The two baluns in the DAC output data paths are for converting the differential output to single ended while suppressing the noise coming from the feedline (the 1:1 balun acts as an isolator). If using only one balun (i.e. the 1:2 balun only), SNR may not be optimal due to noise.
Regards,
Marco