Post Go back to editing

AD9106 DC constant output by run bit?

Category: Datasheet/Specs

WAV4_3CONFIG(Address 0x26) set to 0x0101 (DC constant mode), WAV2_1 CONFIG(Address 0x27) set to 0x3030 (pattern generation mode). If I want to enable the output of Wave4 and Wave3, do I need to set run bit=1? When Run bit=1, controlling the Trigger pin to trigger the pattern generation of Wave2 and 1, will it affect the output of Wave4 and Wave3?

Parents Reply Children