Post Go back to editing

To use the amplifier on the AD9106-ARDZ-EBZ board

Product Number: AD9106-ARDZ-EBZ

Based on the current documentation, I changed the jumper connection as instructed.

Since I only have a 12V/24W wall wart available at the moment, I connected it to P15.

However, I encountered an issue where selecting "On-Board amplifier" in ACE and outputting a waveform did not affect the output voltage, even though I connected the power supply.

Upon reviewing the schematic, I noticed that the VIN of P15 on the board is only connected to the VIN of "POWER".

I am not sure if my understanding is correct.

Vpp originally increased from 400mV to 1.3V (presumably due to the effect of the amplifier on the board),

but I don't understand why it still stays at 1.3V even after connecting the power supply.Thank you.



moved and tagged
[edited by: GenevaCooper at 1:15 PM (GMT -4) on 1 May 2023]

Top Replies

    •  Analog Employees 
    May 2, 2023 in reply to kysih +3 verified

    Hi  ,

    Let me correct my previous statement. The maximum output Vpp of +1.0V is only on the output stage of the AD9106 DAC. The maximum peak-to-peak voltage will increase in the output of the amplifier…

  • Hi  ,

    Can you provide screen captures of your output waveform when you select the "On-board amplifier" in ACE? When outputting a waveform thru the On-board Op-amp, please make sure that the the USB…

Parents Reply Children
  • Hi  

    Can you confirm if you've set the termination to 50Ω for channel 1 in your oscilloscope capture? 

    A:Yes, I have confirmed that the termination for channel 1 in my oscilloscope capture is set to 50Ω.

    But now I'm using the amplifier (ada4817) on the board, and even after amplification, the highest output is only 1V?

  • Hi  ,

    Let me correct my previous statement. The maximum output Vpp of +1.0V is only on the output stage of the AD9106 DAC. The maximum peak-to-peak voltage will increase in the output of the amplifier. The amplifier stage of AD9106 is shown below. This is based on the latest version of AD9106-ARDZ-EBZ Schematic

     

    You are correct: the maximum output Vpp should be around 1.3V. This is assuming the default on-board resistors are used and a typical full-scale current (IOUTFS) of 4mA. The resistances on the amplifier stage can to be changed if a different Vpp is desired, however the resulting output at the AD9106 DAC (IOUTP and IOUTN) should still be within compliance to ensure the performance of the device. 

     

    Regards,


    Marco

  • Hi  

    Thank you very much for your answer!! Now I understand.