Hello,
I have a question about generating a chirp waveform using DPG-Lite.
Our customer wants to generate a complex(I/Q) chirp waveform but the function of "Chirp"
in "Add Generated Waveform" can not generate complex mode.
Therefore he tried two chirp waveforms, one is 0 degrees "Relative phase" and the other is 90 degrees "Relative phase",
and he and I saved the waveforms to check. But the two waveforms are the same. It is not a difference of 90 degrees.
The setting of DPG-Lite is as follows;
The saved data file of "1" and "2" are the same.
Is DPG-Lite not able to adjust a phase in generating a chirp waveform?
Best regards,
y_suzuki