-
I want to use AD9739 instead of AD9735 with the clock unchanged.Can AD9739 be operated in single port mode (e.g. DB1[13:0] unused)?
AD9739
Production
The AD9739 is a 14-bit, 2.5 GSPS high performance RF digital-to-analog converter (DAC) capable of synthesizing wideband
signals from dc up to 3.0 GHz....
Datasheet
AD9739 on Analog.com
AD9735
Production
The AD9736, AD9735, and AD9734 are high performance, high frequency DACs that provide sample rates of up to 1200 MSPS, permitting multicarrier generation...
Datasheet
AD9735 on Analog.com
I want to use AD9739 instead of AD9735 with the clock unchanged.Can AD9739 be operated in single port mode (e.g. DB1[13:0] unused)?
Hi ChenXueWei,
Would you be able to stream the same data into both DB0 and DB1?!
Assumed answered offline.