Post Go back to editing

What is reset value of 0x0026 WAV4_3CONFIG AD9106 register?

Thread Summary

The user encountered issues with reading back registers 0x0026 to 0x3232 incorrectly and receiving a high pulse instead of a sine wave when generating DDS waveforms. The final answer suggested that the issue was resolved offline. The accompanying answer recommended comparing the user's schematics to those in the AD9106 evaluation board documentation and confirmed that all example codes provided in the wiki are working.
AI Generated Content
Category: Software
Product Number: ad9106
Software Version: Latest

Hi,

When I write the registes  0x0026 to 0x3232, I am try to generate DDS waveform using START and STOP delay, after I read back registers, I get the 0x3230. Why these happening three Registes are read wrong. What is exact reset value 0x0026?

I am attaching the execel sheet I put the result in that. I tried to generate DDS through sine wave, but I get the HIGH pulse.

Goal: Four Pulsed Sine Waves with Different Start Delays and Varied Digital Gain Settings Generated by DDS

Issues:

1. When I write and read back the registers three regsiters are read back wrong.

2.On output of four DAC I get the High pulse.

XLSX

Parents Reply Children
No Data