Hi,
When I write the registes 0x0026 to 0x3232, I am try to generate DDS waveform using START and STOP delay, after I read back registers, I get the 0x3230. Why these happening three Registes are read wrong. What is exact reset value 0x0026?
I am attaching the execel sheet I put the result in that. I tried to generate DDS through sine wave, but I get the HIGH pulse.
Goal: Four Pulsed Sine Waves with Different Start Delays and Varied Digital Gain Settings Generated by DDS
Issues:
1. When I write and read back the registers three regsiters are read back wrong.
2.On output of four DAC I get the High pulse.