Post Go back to editing

AD9125_output_waveform

Category: Hardware
Product Number: AD9125

Hello. Please help me.

Q1:output abnormal

 I am seeing anomalies in the output waveform on the AD9125.

 This is happening on the board I designed.

 The figure below shows an abnormal waveform, in which the phase changes at approximately 500ns.

  

 Is there anything I should review in register settings?

 The operation is as follows.

  ・DCI=120MHz

  ・REFCLK=120MHz

  ・Dual-word mode

  ・HB1+HB2=Enable

  ・Internal DACCLK = 480MHz

 I wrote the settings of each register in Excel.

 This phenomenon can sometimes be improved by changing bit6 of 0x0A from "0" → "1" → "0".

Q2:FRAME signal

 Also, the FRAME signal is set to HIGH at the same time as RESET.

 Is there a recommended treatment for the FRAME signal?

Best Regards.

XLSX

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.