Category: Software
Product Number: ad9106
Software Version: STM32
Hello,
I want to generate the continuous DC waveform. Which register I need to configure. Expect 0x27 and 0x31 register which I need to configure.
Because I configure these two registers but no waveform is coming.
1. Make the Reset low and then HIGH. To reset all register DAC.
2. I write the register 0x27 =0101H and 0x30=8000H set gain 0x07=0x4000.
3.Make the Trigger low to start the generating pattern.
But no waveform is coming on DAC1 channel.