Post Go back to editing

AD9735 operating in the second Nyquist zone ?

Category: Hardware
Product Number: AD9735

Hello,

I would like to know if the AD9735 can be operated  with signals in the third Nyquist zone.

In my case, the DAC clock would be 1,2GHz and I need to generate carriers at 1300 MHz ( 5 MHz bandwidth)

I expect to feed the DAC with a signal of 100 MHz and remove the unwanted fundamental and other images with SAW filtering.

Is this possible with AD9735 ? If yes, can we determine roughly the amplitude of that signal that I need ?

Best Regards,

Cristian