Post Go back to editing

Theory. Charged capacitor used to charge an uncharged capacitor. Many contradictions. Any lights welcome.

A relatively old problem since there are "docs" on Internet about the subject, but they suffer major contradictions.

The problem is about a charged capacitor, 1uF, at 5V, used to charge another uncharged capacitor, also 1uF. What are the final voltages? (That it the simplified problem, that is).

First, there is a need to have a resistor, else, the close loop cannot be equilibrated, or the potential cannot exist, choose the one you prefer. Indeed, without resistor, one of the possible paths passes through the 5V and a parallel path, through the same ending points, passes through a total of 0V. So, we need a not-zero resistor in the model to patch that first inconsistency.

Next, the question about if the caps are in series or in parallel. With the necessity of the presence of the resistor, we should cancel any model based on the caps being in parallel.

Finally, there is an argument about keeping the initial Q Coulomb   (  Q = C V  of the initially charged cap) up to the end  ( Q/2  =  C  V_ending, since it is distributed to the 2 caps.) but that leads to loss in energy ( initial 0.5*^2 *C different than  ending:  2*0.5*C*2.5^2 ). Furthermore, with the obliged equation:  Vc1 = Vr + Vc2  (voltage for the caps and the required resistor), the derivative through time leads to  d(Vr) = d(V1) - d(V2).  So, if the total Q must be kept, d(V1)=d(V2)  and thus, the hypothesis lead to Vr = constant. Which is incoherent.

Thanks to still be here, so my question is about if you are aware of a (theorical)  solution which could, among other things, be applicable to back check by hand the solutions of most of the simulators? The simulators do not, in general, consider the energy, since those implies second degree polynomial equations, not as friendly as linear equations, but it would be fine if the solution can also satisfy the conservation of energy,... if possible :-)

Parents
  • More details.

    I started with the well known case of a constant voltage source, Vs. Here are the equations:

    Note that the resistor captures 50% of the initial energy, and that, independently of the value of the resistor (non zero though).

    Knowing that this is a good foundation, basically, all what I have to do for the charged cap case is to replace the energy term in Vs by 1/2  C (V_cap1) ^2. But as I mentioned earlier, that leads me to 3 variables, Vr and the two Vcap, while I have only 2 equations. I don't have that problem with the constant DC source, since then, it is ... a known constant.

Reply
  • More details.

    I started with the well known case of a constant voltage source, Vs. Here are the equations:

    Note that the resistor captures 50% of the initial energy, and that, independently of the value of the resistor (non zero though).

    Knowing that this is a good foundation, basically, all what I have to do for the charged cap case is to replace the energy term in Vs by 1/2  C (V_cap1) ^2. But as I mentioned earlier, that leads me to 3 variables, Vr and the two Vcap, while I have only 2 equations. I don't have that problem with the constant DC source, since then, it is ... a known constant.

Children
No Data