I use the 1.8V output from the ADM7154 to power the VDD_IO of the AD9166. As long as the ADM7154 is connected to the VDD_IO, I measure the output of the ADM7154 to 2.0V. It is normal that the ADM7154 output is not connected. What is the problem?
ADM7154
Recommended for New Designs
TThe ADM7154 is a linear regulator that operates from 2.3 V to
5.5 V and provides up to 600 mA of load current. Using an
advanced proprietary architecture...
Datasheet
ADM7154 on Analog.com
I use the 1.8V output from the ADM7154 to power the VDD_IO of the AD9166. As long as the ADM7154 is connected to the VDD_IO, I measure the output of the ADM7154 to 2.0V. It is normal that the ADM7154 output is not connected. What is the problem?
Before the ADM7154 output was 1.8V, after using the AD9166 for a period of time, the measured output of the ADM7154 became 2.0V. Only 2.0V all the time.
LDO output voltage may rise if the load current is less than 1mA. You can try to add a resistive load to ensure 1mA min load current.
LDO output voltage may rise if the load current is less than 1mA. You can try to add a resistive load to ensure 1mA min load current.