Post Go back to editing

AD9161 JESD204B LMFS=8212 complex sine wave mapping

Category: Hardware
Product Number: AD9161

Hi, I’ve faced with issue with JESD204B mapping for DAC AD9161.

DAC works with following parameters: L = 8; M = 2; N = 16; S = 2; F  = 1.

For data forming, I use INTEL Arria 10GX EVB with JESD204b Intel IP core. IP core was configured with same parameters. I form vector [255:0] with next data order:

I used DPG downloader to generate single tone pattern with next parameters:

 

Relied upon DS for DAC and IP core, I’ve managed octet’s order for both converters:

Octets was forming with using this order (this example for I samples, Q samples are the same):

 

With this configuration, I can’t achieve normal single tone:

Did I make some mistakes or misunderstandings?

Is it correct that with M=2 I need to send complex IQ input data?

 

Parents Reply Children
No Data