I have downloaded hdl-master from GitHub, but I didn't find the example project for ad9154-fmc-ebz
best regards
Edit Notes
Updated form[edited by: GenevaCooper at 1:30 PM (GMT -4) on 6 Jun 2022]
AD9154
Recommended for New Designs
The AD9154 is a quad, 16-bit, high dynamic range digital-to-analog converter (DAC) that provides a maximum sample rate of 2.4 GSPS, permitting multicarrier...
Datasheet
AD9154 on Analog.com
I have downloaded hdl-master from GitHub, but I didn't find the example project for ad9154-fmc-ebz
best regards
Hi xml ,
User guide for this evaluation board in this link: https://wiki.analog.com/resources/eval/dpg/ad9154-ace-fmc-ebz
Or are you asking for a copy of the FPGA source codes?
Regards,
Shine
yes, I am asking for a copy of the fpga source of AD9154-fmc-ebz If allowed
thank you very much! my full name is minglan Xue , email address is xml861119@126.com
Best Regards
thank you ,I have download the source, It's very helpfull to me!
Best Regards
Hello, please create a myAnalog account at analog.com. Let me know once done. Thanks!
Hello,
Could you send me this demo ? Thank you very much. Now I have some problems with AD9154-FMC-EBC & ADS7-V2,There is a physical link between them, but it seems that ADS7 cannot read back the IIC of AD9154-FMC-EBZ, and ADS7 cannot provide 12V power supply when the USB port is not connected. How to solve this problem? my email address is AbyssusZeratul@gmail.com
Hello,
Please send me via direct message the following:
-Full Name
-Email Address used to create a myAnalog account at analog.com.
Regards,
Shine
My full name is Xiangkang and my registered email is AbyssusZeratul@gmail.com