Hello,
I have a question about DAC bandwidth of AD9081/2.
In the datasheet, it indicates "Useable analog bandwidth to 8 GHz" .
But on Table-1 of UG-1578, the "Max Tx Channel Bandwidth (GHz)" of AD9081 is 1.6. I can't figure out the relationship between these two bandwidth.
Does the "Useable analog bandwidth" represents the device bandwidth with CHANNELIZER PATH and MAIN DATA PATH bypass? The "Channel Bandwidth" means using one or both of the PATH?
I want to generate a QPSK intermediate frequency (IF) signal with 2Gsps sample rate, 4GHz IF, 2.5GHz bandwidth, which means the roll-off factor is 0.25. That's no problem if refer to the "Useable analog bandwidth", but it cannot be implemented if refer to the "Channel Bandwidth". Can I generate such a signal with AD9081 or do I have a better device choice?